This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI時鐘極性



我用的是MSP432P401R,我使用官方的範例msp432p401x_euscib0_spi_09撰寫SPI,但我的設備需要將SPI調整為polarity low和'Phase high ,請問我這樣更改是否正確?

    WDT_A->CTL = WDT_A_CTL_PW |             // Stop watchdog timer
            WDT_A_CTL_HOLD;

    P1->OUT &= ~BIT0;
    P1->DIR |= BIT0;                        // Set P1.0 LED

    P1->SEL0 |= BIT5 | BIT6 | BIT7;         // Set P1.5, P1.6, and P1.7 as
                                            // SPI pins functionality

    EUSCI_B0->CTLW0 |= EUSCI_B_CTLW0_SWRST; // Put eUSCI state machine in reset
    EUSCI_B0->CTLW0 = EUSCI_B_CTLW0_SWRST | // Remain eUSCI state machine in reset
            EUSCI_B_CTLW0_MST |             // Set as SPI master
            EUSCI_B_CTLW0_SYNC |            // Set as synchronous mode
            //EUSCI_B_CTLW0_CKPL |            // Set clock polarity high
            EUSCI_B_CTLW0_CKPH |            //Phase high
            EUSCI_B_CTLW0_MSB;              // MSB first

    EUSCI_B0->CTLW0 |= EUSCI_B_CTLW0_SSEL__ACLK; // ACLK
    EUSCI_B0->BRW = 0x01;                   // /2,fBitClock = fBRCLK/(UCBRx+1).
    EUSCI_B0->CTLW0 &= ~EUSCI_B_CTLW0_SWRST;// Initialize USCI state machine