Other Parts Discussed in Thread: CC2650, UNIFLASH
最近在学习contiki os,使用CC26xx Serial Boot Loader来烧录程序到cc2650 LaunchPad,但是需要按下用户按键和重置键,很不方便。(因为下一步要使用树莓派来自动唤醒BSL),网上查阅过资料包括:
- UniFlash的命令行,放弃的原因是不能在树莓派上运行。
- MSP432 BSL Scripter for Linux 32 bit ,好像只能唤醒blank device
- 现在在看这个www.ti.com/.../slau622i.pdf ,发现:
#define BSL_PARAM 0xFC48FFFF // I2C slave address = 0x48, Interface selection = Auto #define BSL_API_TABLE_ADDR 0x00202000 // Address of BSL API table #define BSL_ENTRY_FUNCTION (*((uint32_t *)BSL_API_TABLE_ADDR)) ((void (*)())BSL_ENTRY_FUNCTION)((uint32_t)BSL_PARAM); // Call the BSL with given BSL parameters MAP_Interrupt_disableMaster(); // Setup interrupt priorities into 0x00 before entering bootloader for (int i=0; i < 240; i++) NVIC->IP[i] = 0; NVIC->ICER[0] = 0xFFFF; NVIC->ICPR[0] = 0xFFFF; NVIC->ICER[1] = 0xFFFF; NVIC->ICPR[1] = 0xFFFF; // Call the BSL with given BSL parameters ((void (*)())BSL_ENTRY_FUNCTION)((uint32_t)BSL_PARAM);
但是不知道这个怎么跟contiki的代码结合?