This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129 一个ADC通道下2个序列,只采一个,另一个不进中断



20路ADC全开,定时触发采集。AD0开了SS0采集8路,优先级0,SS1采集4路,优先级1;AD1开了SS0采集8路,优先级2。

现象是AD0的SS0和AD1的SS0都能进中断,AD0的SS1不进中断。把AD0SS1的优先级设为0,AD0SS0优先级调为1后,情况变为AD0的SS1和AD1的SS0都能进中断,AD0的SS0不进中断。

请问一下是什么原因,谢谢!

初始化代码如下:

SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);

//config AIN Pin
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_4 | GPIO_PIN_5);//AIN0-3,AIN8,AIN9

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3 | GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7);//AIN4-7,AIN12-15,

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinTypeADC(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);//AIN10¡¢AIN11

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
GPIOPinTypeADC(GPIO_PORTK_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);//AIN16-19


SysCtlADCSpeedSet(SYSCTL_ADCSPEED_1MSPS);

ADCHardwareOversampleConfigure(ADC0_BASE,16);
ADCHardwareOversampleConfigure(ADC1_BASE,16);



ADCSequenceConfigure(ADC0_BASE, ADC_SS0, ADC_TRIGGER_TIMER, 0);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS0, ADC_STEP0, ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS0, ADC_STEP1, ADC_CTL_CH1);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS0, ADC_STEP2, ADC_CTL_CH2);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS0, ADC_STEP3, ADC_CTL_CH3);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS0, ADC_STEP4, ADC_CTL_CH4);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS0, ADC_STEP5, ADC_CTL_CH5);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS0, ADC_STEP6, ADC_CTL_CH6);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS0, ADC_STEP7, ADC_CTL_CH7 | ADC_CTL_IE | ADC_CTL_END);//

ADCSequenceEnable(ADC0_BASE, ADC_SS0);
ADCIntClear(ADC0_BASE, ADC_SS0); 
ADCIntEnable(ADC0_BASE, ADC_SS0);
IntEnable(INT_ADC0SS0);

ADCSequenceConfigure(ADC0_BASE, ADC_SS1, ADC_TRIGGER_TIMER, 1);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS1, ADC_STEP0, ADC_CTL_CH8);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS1, ADC_STEP1, ADC_CTL_CH9);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS1, ADC_STEP2, ADC_CTL_CH10);
ADCSequenceStepConfigure(ADC0_BASE, ADC_SS1, ADC_STEP3, ADC_CTL_CH11 | ADC_CTL_IE | ADC_CTL_END);


ADCSequenceEnable(ADC0_BASE, ADC_SS1);
ADCIntClear(ADC0_BASE, ADC_SS1);

ADCIntEnable(ADC0_BASE, ADC_SS1);

IntEnable(INT_ADC0SS1);

ADCSequenceConfigure(ADC1_BASE, ADC_SS0, ADC_TRIGGER_TIMER, 2);
ADCSequenceStepConfigure(ADC1_BASE, ADC_SS0, ADC_STEP0, ADC_CTL_CH12);
ADCSequenceStepConfigure(ADC1_BASE, ADC_SS0, ADC_STEP1, ADC_CTL_CH13);
ADCSequenceStepConfigure(ADC1_BASE, ADC_SS0, ADC_STEP2, ADC_CTL_CH14);
ADCSequenceStepConfigure(ADC1_BASE, ADC_SS0, ADC_STEP3, ADC_CTL_CH15);
ADCSequenceStepConfigure(ADC1_BASE, ADC_SS0, ADC_STEP4, ADC_CTL_CH16);
ADCSequenceStepConfigure(ADC1_BASE, ADC_SS0, ADC_STEP5, ADC_CTL_CH17);
ADCSequenceStepConfigure(ADC1_BASE, ADC_SS0, ADC_STEP6, ADC_CTL_CH18);
ADCSequenceStepConfigure(ADC1_BASE, ADC_SS0, ADC_STEP7, ADC_CTL_CH19 | ADC_CTL_IE | ADC_CTL_END);//

ADCSequenceEnable(ADC1_BASE, ADC_SS0);
ADCIntClear(ADC1_BASE, ADC_SS0); 
ADCIntEnable(ADC1_BASE, ADC_SS0);
IntEnable(INT_ADC1SS0);

中断代码如下:

void ADC0_SS0_IntHandler(){
ADCIntClear(ADC0_BASE, ADC_SS0);
Read_ADC0_SS0_Value(); 
}

void ADC0_SS1_IntHandler(){
ADCIntClear(ADC0_BASE, ADC_SS1);
Read_ADC0_SS1_Value();
}

void ADC1_SS0_IntHandler(){
ADCIntClear(ADC1_BASE, ADC_SS0);
Read_ADC1_SS0_Value(); 
}

  • 很抱歉,目前手边没有129的开发板,所以不好测试您的代码。

    但我之前有保存多通道的代码,您可以参考一下

    //*****************************************************************************
    //
    // hello.c - Simple hello world example.
    //
    // Copyright (c) 2013-2014 Texas Instruments Incorporated.  All rights reserved.
    // Software License Agreement
    //
    // Texas Instruments (TI) is supplying this software for use solely and
    // exclusively on TI's microcontroller products. The software is owned by
    // TI and/or its suppliers, and is protected under applicable copyright
    // laws. You may not combine this software with "viral" open-source
    // software in order to form a larger program.
    //
    // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
    // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
    // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
    // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
    // DAMAGES, FOR ANY REASON WHATSOEVER.
    //
    // This is part of revision 2.1.0.12573 of the EK-TM4C1294XL Firmware Package.
    //
    //*****************************************************************************
    
    #include <stdint.h>
    #include <stdbool.h>
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "inc/hw_adc.h"
    #include "inc/hw_timer.h"
    #include "driverlib/gpio.h"
    #include "drivers/pinout.h"
    #include "driverlib/pin_map.h"
    #include "driverlib/rom.h"
    #include "driverlib/rom_map.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/adc.h"
    #include "driverlib/timer.h"
    #include "driverlib/uart.h"
    #include "utils/uartstdio.h"
    
    //*****************************************************************************
    //
    //! \addtogroup example_list
    //! <h1>Hello World (hello)</h1>
    //!
    //! A very simple ``hello world'' example.  It simply displays ``Hello World!''
    //! on the UART and is a starting point for more complicated applications.
    //!
    //! Open a terminal with 115,200 8-N-1 to see the output for this demo.
    //
    //*****************************************************************************
    uint32_t ui32adcValues[4],ui32Count,ui32adc0Values[1],ui32adc1Values[1],ui32adc2Values[1],ui32adc3Values[1];
    
    
    //*****************************************************************************
    //
    // System clock rate in Hz.
    //
    //*****************************************************************************
    uint32_t g_ui32SysClock;
    
    //*****************************************************************************
    //
    // The error routine that is called if the driver library encounters an error.
    //
    //*****************************************************************************
    #ifdef DEBUG
    void
    __error__(char *pcFilename, uint32_t ui32Line)
    {
    }
    #endif
    
    //*****************************************************************************
    //
    // Configure the UART and its pins.  This must be called before UARTprintf().
    //
    //*****************************************************************************
    void
    ConfigureADC(void)
    {
    
    
    		SysCtlPeripheralReset(SYSCTL_PERIPH_GPIOE);
    		SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
    		SysCtlPeripheralReset(SYSCTL_PERIPH_ADC0);
    		SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
    		SysCtlDelay(10);
    
    	    GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0 );
    
    	    ADCClockConfigSet(ADC0_BASE, ADC_CLOCK_SRC_PLL | ADC_CLOCK_RATE_EIGHTH, 30);
    
       	ADCSequenceStepConfigure(ADC0_BASE,0,0, ADC_CTL_CH0);
       	ADCSequenceStepConfigure(ADC0_BASE,0,1, ADC_CTL_CH1);
       	ADCSequenceStepConfigure(ADC0_BASE,0,2, ADC_CTL_CH2);
       	ADCSequenceStepConfigure(ADC0_BASE,0,3, ADC_CTL_CH3 | ADC_CTL_IE | ADC_CTL_END);
    
       	ADCSequenceEnable(ADC0_BASE, 0);
       	ADCSequenceEnable(ADC0_BASE, 1);
       	ADCSequenceEnable(ADC0_BASE, 2);
       	ADCSequenceEnable(ADC0_BASE, 3);
    }
    
    
    uint32_t
    WaitAndReadADC(uint32_t *adcValues)
    {
    
    	ADCProcessorTrigger(ADC0_BASE,0);
        // Wait until the sample sequence has completed.
    
        while(!ADCIntStatus(ADC0_BASE, 0, false)) { }
        // Read the value from the ADC.
    
    
        return(ADCSequenceDataGet(ADC0_BASE, 0, adcValues));
    }
    
    
    uint32_t
    WaitAndReadADC1(uint32_t *adcValues)
    {
    
    	ADCProcessorTrigger(ADC0_BASE,1);
        // Wait until the sample sequence has completed.
    
        while(!ADCIntStatus(ADC0_BASE, 1, false)) { }
        // Read the value from the ADC.
    
    
        return(ADCSequenceDataGet(ADC0_BASE, 1, adcValues));
    }
    
    uint32_t
    WaitAndReadADC2(uint32_t *adcValues)
    {
    
    	ADCProcessorTrigger(ADC0_BASE,2);
        // Wait until the sample sequence has completed.
    
        while(!ADCIntStatus(ADC0_BASE, 2, false)) { }
        // Read the value from the ADC.
    
    
        return(ADCSequenceDataGet(ADC0_BASE, 2, adcValues));
    }
    
    uint32_t
    WaitAndReadADC3(uint32_t *adcValues)
    {
    
    	ADCProcessorTrigger(ADC0_BASE,3);
        // Wait until the sample sequence has completed.
    
        while(!ADCIntStatus(ADC0_BASE, 3, false)) { }
        // Read the value from the ADC.
    
    
        return(ADCSequenceDataGet(ADC0_BASE, 3, adcValues));
    }
    
    
    //*****************************************************************************
    //
    // Print "Hello World!" to the UART on the Intelligent UART Module.
    //
    //*****************************************************************************
    int
    main(void)
    {
    
        //
        // Run from the PLL at 120 MHz.
        //
        g_ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                    SYSCTL_OSC_MAIN | SYSCTL_USE_PLL |
                    SYSCTL_CFG_VCO_480), 120000000);
    
        //
        // Configure the device pins.
        //
        PinoutSet();
    
        //
        // Enable the GPIO pins for the LED D1 (PN1).
        //
        ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_1);
    
        //
        // Initialize the UART.
        //
        ConfigureADC();
    
        //
        // Hello!
        //
    
    
        //
        // We are finished.  Hang around flashing D1.
        //
        while(1)
        {
    
    
    
            //
            // Turn on D1.
            //
            //LEDWrite(CLP_D1, 1);
         	//ui32Count = WaitAndReadADC0(ui32adc0Values);
         	//ui32Count = WaitAndReadADC1(ui32adc1Values);
         	//ui32Count = WaitAndReadADC2(ui32adc2Values);
         	ui32Count = WaitAndReadADC(ui32adcValues);
    
    
    
            //
            // Delay for a bit.
            //
           // SysCtlDelay(g_ui32SysClock / 10 / 3);
    
            //
            // Turn off D1.
            //
            //LEDWrite(CLP_D1, 0);
    
            //
            // Delay for a bit.
            //cank
           // SysCtlDelay(g_ui32SysClock / 10 / 3);
        }
    }
    

    参考链接为 https://e2e.ti.com/support/microcontrollers/other/f/908/t/476214#pi320995=1