This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART 发送数据时有时会接收到数据



TM4C1294 使用 UART2 口, 接485 芯片, 使用直接写寄存器方式send 数据, 有时在 send 完数据后,会导致  UART 寄存器 RXFE 被置为 0 , 也即是接收到了数据,请问这是什么问题?

如果单步执行,还没有发现 RXFE 被置为0 ,如果全速运行,30% 的可能性。

代码里 send 第一步是设置 485 为发送模式。

void _UARTSend(uint8_t index,const uint8_t *pui8Data, uint32_t ui32Size)
{
 

    HWREG(uart_normal_setting[index].UART_GPIO_Port + (GPIO_O_DATA + (uart_normal_setting[index].UART_GPIO_SR_PIN << 2))) = uart_normal_setting[index].UART_GPIO_SR_PIN;
    while(ui32Size--)
    {
        //
        // Make sure that the transmit FIFO is not full.
        //
        while((HWREG(uart_udma_setting[index].UART_BASE + UART_O_FR) & UART_FR_TXFF))
        {
        }

        //
        // Send out the next byte.
        //
        HWREG(uart_udma_setting[index].UART_BASE + UART_O_DR) = *pui8Data++;
    }


    //
    // Wait until the UART is done transmitting.
    //
    _UARTFlush(index);
   
}
void _UARTFlush(uint8_t index)
{
    //
    // Wait for the UART FIFO to empty and then wait for the shifter to get the
    // bytes out the port.
    //
    while(!(HWREG(uart_udma_setting[index].UART_BASE + UART_O_FR) & UART_FR_TXFE))
    {
    }

    //
    // Wait for the FIFO to not be busy so that the shifter completes.
    //
    while((HWREG(uart_udma_setting[index].UART_BASE + UART_O_FR) & UART_FR_BUSY))
    {
    }
}