Other Parts Discussed in Thread: UNIFLASH
TMS320F28335PTPQ在烧写出现图中所述故障
Load program error.
File:
F:/helz\JCWT51-062_Software_v1.00\Debug\JCWT51-062_Software_v
1.00.out:a data verification error occurred, file load failed
Error connecting to the target
(Err-233@0x0)
The JTAG IR and DR scan-paths cannot circulate bits,they may be broken.
An attempt to scan the JTAG scan-path has failed
The target's TJAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault
这2个是TJAG烧写出现的问题
***PLEASE RESET TARGET IN SCI BOOT-LOADER MODE***
Connecting with target(autobaud)...OK.
Bootloading...OK.
Please wait...
Connecting with target...
-Chip ID:0xEF
-Chip Rev:0x01
OK.
Unlocking target...failed(wrong key)!
这个是串口烧写出现的问题!
有遇见一样问题的,麻烦帮忙协助一下类似案例,谢谢!