This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求帮写一个用tm4c129encpdtTIMER例程写的中断程序控制小灯闪烁,万分感谢



//*****************************************************************************
//
// timers.c - Timers example.
//
// Copyright (c) 2013 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
// 
// Texas Instruments (TI) is supplying this software for use solely and
// exclusively on TI's microcontroller products. The software is owned by
// TI and/or its suppliers, and is protected under applicable copyright
// laws. You may not combine this software with "viral" open-source
// software in order to form a larger program.
// 
// THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS.
// NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT
// NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY
// CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL
// DAMAGES, FOR ANY REASON WHATSOEVER.
// 
// This is part of revision 2.0.1.11577 of the DK-TM4C129X Firmware Package.
//
//*****************************************************************************

#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/interrupt.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
#include "grlib/grlib.h"
#include "drivers/frame.h"
#include "drivers/kentec320x240x16_ssd2119.h"
#include "drivers/pinout.h"

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Timer (timers)</h1>
//!
//! This example application demonstrates the use of the timers to generate
//! periodic interrupts.  One timer is set up to interrupt once per second and
//! the other to interrupt twice per second; each interrupt handler will toggle
//! its own indicator on the display.
//
//*****************************************************************************

//*****************************************************************************
//
// Flags that contain the current value of the interrupt indicator as displayed
// on the display.
//
//*****************************************************************************
uint32_t g_ui32Flags;

//*****************************************************************************
//
// Graphics context used to show text on the display.
//
//*****************************************************************************
tContext g_sContext;

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// The interrupt handler for the first timer interrupt.
//
//*****************************************************************************
void
Timer0IntHandler(void)
{
    //
    // Clear the timer interrupt.
    //
    ROM_TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);

    //
    // Toggle the flag for the first timer.
    //
    HWREGBITW(&g_ui32Flags, 0) ^= 1;




//*****************************************************************************
//
// This example application demonstrates the use of the timers to generate
// periodic interrupts.
//
//*****************************************************************************
int
main(void)
{
    uint32_t ui32SysClock;

    //
    // Run from the PLL at 120 MHz.
    //
    ui32SysClock = SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
                                       SYSCTL_OSC_MAIN |
                                       SYSCTL_USE_PLL |
                                       SYSCTL_CFG_VCO_480), 120000000);

    //
    // Configure the device pins.
    //
    PinoutSet();


    // Enable the peripherals used by this example.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);


    //
    // Enable processor interrupts.
    //
    ROM_IntMasterEnable();

    //
    // Configure the two 32-bit periodic timers.���ö�ʱ������ʱ�����ͣ��趨��ַ���ƶ�timer���趨����
    //
    ROM_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
    ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, ui32SysClock);

    //
    // Setup the interrupts for the timer timeouts.ʹ�ܳ�ʱ�ж�
    //
    ROM_IntEnable(INT_TIMER0A);
    ROM_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);

    //
    // Enable the timers.���timer��ʼ����
    //
    ROM_TimerEnable(TIMER0_BASE, TIMER_A);

    //
    // Loop forever while the timers run.
    //
    while(1)
    {
    }
}
//*****************************************************************************
//
// project.c - Simple project to use as a starting point for more complex
//             projects.
//
// Copyright (c) 2013 Texas Instruments Incorporated.  All rights reserved.
// Software License Agreement
// 
//   Redistribution and use in source and binary forms, with or without
//   modification, are permitted provided that the following conditions
//   are met:
// 
//   Redistributions of source code must retain the above copyright
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the
//   documentation and/or other materials provided with the  
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// 
// This is part of revision 2.0.1.11577 of the Tiva Firmware Development Package.
//
//*****************************************************************************

#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/rom.h"
#include "driverlib/sysctl.h"

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>Simple Project (project)</h1>
//!
//! A very simple example that can be used as a starting point for more complex
//! projects.  Most notably, this project is fully TI BSD licensed, so any and
//! all of the code (including the startup code) can be used as allowed by that
//! license.
//!
//! The provided code simply toggles a GPIO using the Tiva Peripheral Driver
//! Library.
//
//*****************************************************************************

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// Toggle a GPIO.
//
//*****************************************************************************
int
main(void)
{
    //
    // Enable the GPIO module.
    //
    ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
    ROM_SysCtlDelay(1);

    //
    // Configure PA1 as an output.
    //
    ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);

    //
    // Loop forever.
    //
    while(1)
    {
        //
        // Set the GPIO high.
        //
        ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);

        //
        // Delay for a while.
        //
        ROM_SysCtlDelay(1000000);

        //
        // Set the GPIO low.
        //
        ROM_GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);

        //
        // Delay for a while.
        //
        ROM_SysCtlDelay(1000000);
    }
}

这两个是分别控制超时中断和延时闪烁的程序,万分感谢!!