This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PM--ADC多通道采样



我在实验过程中通过ADCSS0采了8条通道,其中7道都接地,CH6采集3V电压。最后通过串口输出发现CH6(3V)对应的数据不在pui32ADC0Value[6]的位置。

void ADC0Init()
{
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);             
  GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0);
        
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
  GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0);    
   
  ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_ALWAYS, 0);
    
    //
    // Configure step 0--7 on sequence 0.  
    //
    ADCSequenceStepConfigure(ADC0_BASE, 0, 0, ADC_CTL_CH0);
    ADCSequenceStepConfigure(ADC0_BASE, 0, 1, ADC_CTL_CH1);
    ADCSequenceStepConfigure(ADC0_BASE, 0, 2, ADC_CTL_CH2);
    ADCSequenceStepConfigure(ADC0_BASE, 0, 3, ADC_CTL_CH3);
    ADCSequenceStepConfigure(ADC0_BASE, 0, 4, ADC_CTL_CH4);
    ADCSequenceStepConfigure(ADC0_BASE, 0, 5, ADC_CTL_CH5);
    ADCSequenceStepConfigure(ADC0_BASE, 0, 6, ADC_CTL_CH6);
    ADCSequenceStepConfigure(ADC0_BASE, 0, 7, ADC_CTL_CH7 | ADC_CTL_IE | ADC_CTL_END );
    
    
    //
    // enable ADC0 sequence 0 interrupt
    //
    ADCIntEnable(ADC0_BASE, 0);
    
    //IntEnable(INT_ADC0SS0);
    IntMasterEnable();
    ADCSequenceEnable(ADC0_BASE, 0);
    ADCIntClear(ADC0_BASE, 0);
}   

while(1)
    {            
            while(!ADCIntStatus(ADC0_BASE,0,true));
            ADCSequenceDisable(ADC0_BASE,0);    
            
            ADCSequenceDataGet(ADC0_BASE, 0, pui32ADC0Value);

            for(i = 0; i < 8; i++)  
            {
                UARTprintf("%d(%d),",pui32ADC0Value[i],i);
            }
            UARTprintf("  --\n");
            
            ADCSequenceEnable(ADC0_BASE,0);
            ADCIntClear(ADC0_BASE, 0);
        }

经过修改之后发现在while循环中进入中断后先关闭ADCSS0,最后再使能加清楚中断标志,这个数据就不会乱串,但是位置还是不对,CH6的数据跑到了pui32ADC0Value[5],换了个通道采同样还是数据会靠前一位输出。