Other Parts Discussed in Thread: MSP432WARE
我在使用MSP432的定时器触发SPI通信的中断中,设置通信频率为1M,但是实际测试通信频率达不到1M,测试发现在中断中调用API函数花费过多时间,我想操作寄存器来代替API函数,但是NVIC的寄存器实在是难于理解。
可以的话,希望能解答一下 MAP_TimerIntClear(TIMER2_BASE, TIMER_TIMB_TIMEOUT)函数的寄存器操作
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: MSP432WARE
我在使用MSP432的定时器触发SPI通信的中断中,设置通信频率为1M,但是实际测试通信频率达不到1M,测试发现在中断中调用API函数花费过多时间,我想操作寄存器来代替API函数,但是NVIC的寄存器实在是难于理解。
可以的话,希望能解答一下 MAP_TimerIntClear(TIMER2_BASE, TIMER_TIMB_TIMEOUT)函数的寄存器操作
图片中对应的是core_cm4.h的以下代码,您可以给下面的定义来赋值的
/**
\ingroup CMSIS_core_register
\defgroup CMSIS_NVIC Nested Vectored Interrupt Controller (NVIC)
\brief Type definitions for the NVIC Registers
@{
*/
/**
\brief Structure type to access the Nested Vectored Interrupt Controller (NVIC).
*/
typedef struct
{
__IOM uint32_t ISER[8U]; /*!< Offset: 0x000 (R/W) Interrupt Set Enable Register */
uint32_t RESERVED0[24U];
__IOM uint32_t ICER[8U]; /*!< Offset: 0x080 (R/W) Interrupt Clear Enable Register */
uint32_t RSERVED1[24U];
__IOM uint32_t ISPR[8U]; /*!< Offset: 0x100 (R/W) Interrupt Set Pending Register */
uint32_t RESERVED2[24U];
__IOM uint32_t ICPR[8U]; /*!< Offset: 0x180 (R/W) Interrupt Clear Pending Register */
uint32_t RESERVED3[24U];
__IOM uint32_t IABR[8U]; /*!< Offset: 0x200 (R/W) Interrupt Active bit Register */
uint32_t RESERVED4[56U];
__IOM uint8_t IP[240U]; /*!< Offset: 0x300 (R/W) Interrupt Priority Register (8Bit wide) */
uint32_t RESERVED5[644U];
__OM uint32_t STIR; /*!< Offset: 0xE00 ( /W) Software Trigger Interrupt Register */
} NVIC_Type;