This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TDA4 网络问题(ti-processor-sdk-rtos-j721e-evm-07_03_00_07.tar)

请问ti-processor-sdk-rtos-j721e-evm-07_03_00_07.tar包中ti-processor-sdk-rtos-j721e-evm-07_03_00_07/pdk_jacinto_07_03_00_29/packages/ti/transport/ndk/nimu/example这个例子能正常运行吗?

我用sbl启动方式,运行后在上位机ping不通,请问什么原因?感谢!

  • 请问您使用是哪款芯片?若是使用的是处理器的话,请您发帖至处理器论坛:

    e2echina.ti.com/.../
  • 我用的是TDA4 evm评估板,上面是自带的芯片。
  • 我用的是TDA4评估板。
    MCU_ENET
    –DP83867 RGMII PHY
    –1 Gbps
    –CPSW 2G MDIO bus
  • 谢谢反馈。您可以将帖子发至 处理器 论坛,但一般该型号是国外工程师来支持的,最好发至英文论坛

    e2e.ti.com/.../processors-forum
  • 运行文档中8.5.6.3. Run Enet NIMU example (TCP/IP example)这个例子发现报一下错误。

    请问是什么原因?

    [16:43:31:112] EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 1 To 0 ␍␍␊

    [16:43:31:208] EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:4 From 1 To 0 ␍␍␊

    [16:43:31:304] CPSW_9G Test on MAIN NAVSS␍␍␊

    [16:43:31:336] EnetBoard_setupPorts: 1 of 1 ports configurations found␍␍␊

    [16:43:31:400] EnetPhy_bindDriver: PHY 0: OUI:080028 Model:23 Ver:01 <-> 'dp83867' : OK␍␍␊

    [16:43:31:464] PHY 0 is alive␍␍␊

    [16:43:31:480] EnetUdma_allocRingMon: Ring monitor alloc failed Status=0xfffffff8␍␍␊

    [16:43:31:560] [UDMA] Assertion @ Line: 1082 in src/udma_event.c: monHandle->ringMonNum != UDMA_RING_MON_INVALID : failed !!!␍␍␊

    [16:43:31:672] [UDMA] [Error] Sciclient event config failed!!!␍␍␊

    [16:43:31:720] [UDMA] [Error] Event config failed!!␍␍␊

    [16:43:31:752] EnetDma_openRxCh: [Enet UDMA] Rx Flow Open: event registration failed!!: 0xffffffff␍␍␊

    [16:43:31:832] EnetDma_openRxCh: Assertion @ Line: 497 in src/dma/udma/enet_udma.c: UDMA_SOK == retVal␍␍␊

  • 如之前所说,请将帖子发至 处理器 论坛,但一般该型号是国外工程师来支持的,最好发至英文论坛