This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GXL: 请教使用二片EK-TM4C123GXL,做SPI(SSI)通讯问题

Part Number: EK-TM4C123GXL

TI各位好:
想使用二片板子做SSI通讯,其中遇到问题。

问题1:当Master没发送SSIDataPut,量测CLK没有讯号。有发送SSIDataPut,才会量测到CLK讯号。这样是否正常?

问题2:当SLAVE未收到CLK,是不是不会工作,因为Debug时,发现程式跑完设定参数完后就停止。

目前我Master程式是在While(1)迴圈內打SSIDataPut,才會有一直有CLK出現。

  • 您可以看一下 tivaware的安装文件夹内 ti\TivaWare_C_Series-2.1.4.178\driverlib 以及 C:\ti\TivaWare_C_Series-2.1.4.178\examples\peripherals\ssi 内的SSI的驱动

    具体连接您可以参考

    Clk-Clk

    Fss-Fss

    Tx-Rx

    Rx-Tx

  • 感谢回覆,但是还有一些问题想提问,问题1:想询问Slave传送资料至Master时机,我测试时Master接收到资料是错误的。
    问题2: FSS接脚还需要额外去控制H,L吗?
  • 问题1:想询问Slave传送资料至Master时机,我测试时Master接收到资料是错误的。

    能否详细说明一下?另外您是否有使用示波器观察总线上的情况?

    问题2: FSS接脚还需要额外去控制H,L吗?

    理论上不需要的

  • 程式内查看Master和Slave接收资料状况,Slave接收Master资料是正确,但Master接收Slave资料是错误。

    下图黄色波形是FSS和蓝色波形是Master-RX。

    Master和Slave程式如下:

    SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
    GPIOPinConfigure(GPIO_PA2_SSI0CLK);
    GPIOPinConfigure(GPIO_PA3_SSI0FSS);
    GPIOPinConfigure(GPIO_PA4_SSI0RX);
    GPIOPinConfigure(GPIO_PA5_SSI0TX);
    GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_5 | GPIO_PIN_4 | GPIO_PIN_3 |GPIO_PIN_2);
    while(!SysCtlPeripheralReady(SYSCTL_PERIPH_SSI0))
    {
    }
    SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
    SSI_MODE_MASTER ,500000, 8);
    //SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
    //SSI_MODE_SLAVE,500000, 8);
    SSIEnable(SSI0_BASE);
    IntEnable(INT_SSI0);

    while(1)
    {

    for(ui32Index = 0; ui32Index <5; ui32Index++)
    {
    SSIDataPut(SSI0_BASE, pui32DataTx[ui32Index]);
    SSIDataGet(SSI0_BASE, &pui32DataRx[ui32Index]);
    }
    while(SSIBusy(SSI0_BASE))
    {
    }
    }

  • 建议您在将

    for(ui32Index = 0; ui32Index <5; ui32Index++)
    {
    SSIDataPut(SSI0_BASE, pui32DataTx[ui32Index]);
    SSIDataGet(SSI0_BASE, &pui32DataRx[ui32Index]);
    }

    替换为类似下面的代码

    //
    // Send 3 bytes of data.
    //
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
    //
    // Display the data that SSI is transferring.
    //
    UARTprintf("'%c' ", pui32DataTx[ui32Index]);

    //
    // Send the data using the "blocking" put function. This function
    // will wait until there is room in the send FIFO before returning.
    // This allows you to assure that all the data you send makes it into
    // the send FIFO.
    //
    SSIDataPut(SSI0_BASE, pui32DataTx[ui32Index]);
    }

    //
    // Wait until SSI0 is done transferring all the data in the transmit FIFO.
    //
    while(SSIBusy(SSI0_BASE))
    {
    }

    //
    // Display indication that the SSI is receiving data.
    //
    UARTprintf("\nReceived:\n ");

    //
    // Receive 3 bytes of data.
    //
    for(ui32Index = 0; ui32Index < NUM_SSI_DATA; ui32Index++)
    {
    //
    // Receive the data using the "blocking" Get function. This function
    // will wait until there is data in the receive FIFO before returning.
    //
    SSIDataGet(SSI0_BASE, &pui32DataRx[ui32Index]);

    //
    // Since we are using 8-bit data, mask off the MSB.
    //
    pui32DataRx[ui32Index] &= 0x00FF;

    //
    // Display the data that SSI0 received.
    //
    UARTprintf("'%c' ", pui32DataRx[ui32Index]);
    }

  • 感谢回覆,后来测试我更改成如下程式,且FSS功能利用GPIO输出H、L去代替。
    另外我也做了和Playstation 2 Controller連線控制,也能接收到資料。 while(1) { while(SSIDataGetNonBlocking(SSI0_BASE, &pui32DataRx[0])) { } GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_6,~GPIO_PIN_6); //SysCtlDelay((SysCtlClockGet() / (6500000))); for(SSI_i = 0; SSI_i<5; SSI_i++) { SSIDataPut(SSI0_BASE, pui32DataTx[SSI_i]); SysCtlDelay((SysCtlClockGet() / (40000))); } while(SSIBusy(SSI0_BASE)) { } //SysCtlDelay((SysCtlClockGet() / (5000000))); GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_6,GPIO_PIN_6); SysCtlDelay((SysCtlClockGet() / (50000))); for(SSI_j = 0; SSI_j <5; SSI_j++) { SSIDataGet(SSI0_BASE, &pui32DataRx[SSI_j]); pui32DataRx[SSI_j] &= 0x00FF; } }
  • 谢谢您的反馈,很高兴您能解决问题