This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
1. 在demo code里面的startup.c文件和HALCON自动生成的HL_startup.c文件有什么区别?
2. 在uart_bootloader中,我看英文论坛里面说要把F021_API为什么要从flash里面copy到SRAM中?是为了提高api的运行速度还是什么?这里的SRAM就是指片内的RAM吧?
startup.c文件和HALCON自动生成的HL_startup.c文件有什么区别?
理论上两者的功能是相同的,我会在周一再次确认一下
把F021_API为什么要从flash里面copy到SRAM中
某些特殊情况下,我们需要在程序运行的初始阶段将代码段指令从拷贝到RAM或者SDRAM的指定位置,然后让CPU每次从RAM或者SDRAM取执行并执行。例如: