Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
TMS570LC4357配置SCI发送的DMA后,无法发送出数据。
具体代码:
uint32 SCI1_TX_DATA[32]={0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x33,0x33};
dmaReqAssign(DMA_CH0, 29);
g_dmaCTRLPKT.SADD = (uint32)(&SCI1_TX_DATA) ; /* source address */
g_dmaCTRLPKT.DADD = (uint32_t)(&(sciREG1->TD)); /* destination address */
g_dmaCTRLPKT.CHCTRL = 0;
g_dmaCTRLPKT.FRCNT = 8;
g_dmaCTRLPKT.ELCNT = 1; /* element destination offset */
g_dmaCTRLPKT.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT.PORTASGN = 4;
g_dmaCTRLPKT.RDSIZE = ACCESS_32_BIT; /* read size */
g_dmaCTRLPKT.WRSIZE = ACCESS_32_BIT; /* write size */
g_dmaCTRLPKT.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT.ADDMODEWR = ADDR_FIXED; /* address mode write */
g_dmaCTRLPKT.AUTOINIT = AUTOINIT_ON; /* auto init */
dmaSetCtrlPacket(DMA_CH0,g_dmaCTRLPKT);
dmaSetChEnable(DMA_CH0, DMA_HW);
sciREG1->SETINT = SCI_SET_TX_DMA;
串口没有发出数据。