This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: SCI1 DMA 数据发送不出去

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

TMS570LC4357配置SCI发送的DMA后,无法发送出数据。

具体代码:

uint32 SCI1_TX_DATA[32]={0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x30,0x31,0x32,0x33,0x34,0x35,0x36,0x37,0x38,0x39,0x33,0x33};

dmaReqAssign(DMA_CH0, 29);
g_dmaCTRLPKT.SADD = (uint32)(&SCI1_TX_DATA) ; /* source address */
g_dmaCTRLPKT.DADD = (uint32_t)(&(sciREG1->TD)); /* destination address */
g_dmaCTRLPKT.CHCTRL = 0;
g_dmaCTRLPKT.FRCNT = 8;
g_dmaCTRLPKT.ELCNT = 1; /* element destination offset */
g_dmaCTRLPKT.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT.PORTASGN = 4;
g_dmaCTRLPKT.RDSIZE = ACCESS_32_BIT; /* read size */
g_dmaCTRLPKT.WRSIZE = ACCESS_32_BIT; /* write size */
g_dmaCTRLPKT.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT.ADDMODEWR = ADDR_FIXED; /* address mode write */
g_dmaCTRLPKT.AUTOINIT = AUTOINIT_ON; /* auto init */

dmaSetCtrlPacket(DMA_CH0,g_dmaCTRLPKT);

dmaSetChEnable(DMA_CH0, DMA_HW);


sciREG1->SETINT = SCI_SET_TX_DMA;

串口没有发出数据。

  • 对于数据发送,您可以使用 TXRDY flag . 当 SCI 将 SCITD 的内容传输到 SCITXSHF 时,TXRDY 标志被设置。

    对于 SCI 接收,您可以使用 RXRDY 标志来启动 DMA 传输。当 SCI 将新接收的数据从 SCIRXSHF 寄存器传输到 SCIRD 缓冲区时,RXRDY 标志被设置。 

  • DMA无法将数据移到SCI的TD和移出RD。是什么原因?

  • 我们有一个sci dma的例程,您是否有参考?

    HALCoGen\v04.07.01\examples\TMS570LC43x

    /** @example example_sci_dma.c
    *   This is an example which descibes the steps to create an example application which
    *   configures SCI transfer using DMA. The transmit buffer of the Mibspi RAM is
    *   loaded with data through the DMA.
    *
    *   @b Step @b 1:
    *
    *   Create a new project.
    *
    *   Navigate: -> File -> New -> Project
    *
    *   @image html example_createProject.jpg "Figure: Create a new Project"
    *
    *   @b Step @b 2:
    *
    *   Configure driver code generation:
    *   - Enable SCI driver
    *   - Disable others
    *
    *   Navigate: -> TMS570LCxx /RM5x -> Enable Drivers
    *
    *   @b Step @b 3:
    *
    *   Configure SCI3:
    *
    *   Navigate: -> TMS570Lxx /RMx -> SCI3
    *
    *   @image html sci_uart.JPG   "Figure: SCI Global settings"
    *
    *
    *   @image html sci_uart1.JPG  "Figure: SCI Data Format"
    *
    *   The example file example_sciDma.c can also be found in the examples folder: ../HALCoGen/examples
    *
    *   @note HALCoGen generates an enpty main function in sys_main.c,
    *         please make sure that you link in the right main function or copy the source into the user code sections of this file.
    *
    */
    
    
    /* 
    * Copyright (C) 2009-2015 Texas Instruments Incorporated - www.ti.com
    * 
    * 
    *  Redistribution and use in source and binary forms, with or without 
    *  modification, are permitted provided that the following conditions 
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright 
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the 
    *    documentation and/or other materials provided with the   
    *    distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES INCLUDING, BUT NOT 
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    *  INCLUDING NEGLIGENCE OR OTHERWISE ARISING IN ANY WAY OUT OF THE USE 
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    */
    
    /* USER CODE BEGIN (0) */
    /* USER CODE END */
    
    /* Include Files */
    
    #include "HL_sys_common.h"
    #include "HL_system.h"
    
    /* USER CODE BEGIN (1) */
    #include "HL_sys_dma.h"
    #include "HL_sci.h"
    #include "stdio.h"
    /* USER CODE END */
    
    /** @fn void main(void)
    *   @brief Application main function
    *   @note This function is empty by default.
    *
    *   This function is called after startup.
    *   The user can use this function to implement the application.
    */
    
    /* USER CODE BEGIN (2) */
    #define size 100
    /* External connection (SCI3 TX -> SCI4 RX) is needed in case LOOPBACKMODE is defined as 0 */
    #define LOOPBACKMODE 1
    
    /* Tx and Rx data buffer */
    uint8_t TX_DATA[size], RX_DATA[size] = {0};
    
    /* Addresses of SCI 8-bit TX/Rx data */
    #if ((__little_endian__ == 1) || (__LITTLE_ENDIAN__ == 1))
    #define SCI3_TX_ADDR ((uint32_t)(&(sciREG3->TD)))
    #define SCI3_RX_ADDR ((uint32_t)(&(sciREG3->RD)))
    #define SCI4_TX_ADDR ((uint32_t)(&(sciREG4->TD)))
    #define SCI4_RX_ADDR ((uint32_t)(&(sciREG4->RD)))
    #else
    #define SCI3_TX_ADDR ((uint32_t)(&(sciREG3->TD)) + 3)
    #define SCI3_RX_ADDR ((uint32_t)(&(sciREG3->RD)) + 3)
    #define SCI4_TX_ADDR ((uint32_t)(&(sciREG4->TD)) + 3)
    #define SCI4_RX_ADDR ((uint32_t)(&(sciREG4->RD)) + 3)
    #endif
    
    #define DMA_SCI3_TX  DMA_REQ31
    #define DMA_SCI3_RX  DMA_REQ30
    #define DMA_SCI4_TX  DMA_REQ43
    #define DMA_SCI4_RX  DMA_REQ42
    
    #define SCI_SET_TX_DMA      (1<<16)
    #define SCI_SET_RX_DMA      (1<<17)
    #define SCI_SET_RX_DMA_ALL  (1<<18)
    /* USER CODE END */
    
    uint8	emacAddress[6U] = 	{0xFFU, 0xFFU, 0xFFU, 0xFFU, 0xFFU, 0xFFU};
    uint32 	emacPhyAddress	=	0U;
    
    void main(void)
    {
    /* USER CODE BEGIN (3) */
    	uint32 sciTxData, sciRxData;
    	int i;
    	g_dmaCTRL g_dmaCTRLPKT1, g_dmaCTRLPKT2;
    
    	/*Load source data*/
    	for (i=0; i<size; i++)
    	{
    		TX_DATA[i] = i;
    	}
    
    	/*Initialize SCI*/
    	sciInit();
    
    #if LOOPBACKMODE == 1
    	/* Enable SCI loopback */
    	sciEnableLoopback(sciREG3, Digital_Lbk);
    	while (((sciREG3->FLR & SCI_TX_INT) == 0U) || ((sciREG3->FLR & 0x4) == 0x4))
        {
    	} /* Wait */
    
    	/*Assign DMA request SCI3 transmit to Channel 0*/
    	dmaReqAssign(DMA_CH0, DMA_SCI3_TX);
    
    	/*Assign DMA request SCI3 receive to Channel 1*/
    	dmaReqAssign(DMA_CH1, DMA_SCI3_RX);
    
    	sciTxData = SCI3_TX_ADDR;
    	sciRxData = SCI3_RX_ADDR;
    
    #else
    	while (((sciREG3->FLR & SCI_TX_INT) == 0U) || ((sciREG3->FLR & 0x4) == 0x4))
        {
    	} /* Wait */
    
    	/*Assign DMA request SCI3 transmit to Channel 0*/
    	dmaReqAssign(DMA_CH0, DMA_SCI3_TX);
    
    	/*Assign DMA request SCI4 receive to Channel 1*/
    	dmaReqAssign(DMA_CH1, DMA_SCI4_RX);
    
    	sciTxData = SCI3_TX_ADDR;
    	sciRxData = SCI4_RX_ADDR;
    
    #endif
    
    	/*Configure control packet for Channel 0*/
    	g_dmaCTRLPKT1.SADD      = (uint32_t)TX_DATA;	/* source address             */
    	g_dmaCTRLPKT1.DADD      = sciTxData;		    /* destination  address       */
    	g_dmaCTRLPKT1.CHCTRL    = 0;                	/* channel control            */
    	g_dmaCTRLPKT1.FRCNT	   = size;                  /* frame count                */
    	g_dmaCTRLPKT1.ELCNT     = 1;             	    /* element count              */
    	g_dmaCTRLPKT1.ELDOFFSET = 0;                	/* element destination offset */
    	g_dmaCTRLPKT1.ELSOFFSET = 0;		          	/* element destination offset */
    	g_dmaCTRLPKT1.FRDOFFSET = 0;		          	/* frame destination offset   */
    	g_dmaCTRLPKT1.FRSOFFSET = 0;                	/* frame destination offset   */
    	g_dmaCTRLPKT1.PORTASGN  = PORTA_READ_PORTB_WRITE;
    	g_dmaCTRLPKT1.RDSIZE    = ACCESS_8_BIT;		    /* read size                  */
    	g_dmaCTRLPKT1.WRSIZE    = ACCESS_8_BIT;	 	    /* write size                 */
    	g_dmaCTRLPKT1.TTYPE     = FRAME_TRANSFER;  	    /* transfer type              */
    	g_dmaCTRLPKT1.ADDMODERD = ADDR_INC1;        	/* address mode read          */
    	g_dmaCTRLPKT1.ADDMODEWR = ADDR_FIXED;      	    /* address mode write         */
    	g_dmaCTRLPKT1.AUTOINIT  = AUTOINIT_OFF;      	/* autoinit                   */
    
    	/*Configure control packet for Channel 1*/
    	g_dmaCTRLPKT2.SADD      = sciRxData;	        /* source address             */
    	g_dmaCTRLPKT2.DADD      = (uint32_t)RX_DATA;	/* destination  addr ss       */
    	g_dmaCTRLPKT2.CHCTRL    = 0;                	/* channel control            */
    	g_dmaCTRLPKT2.FRCNT	   = size;                  /* frame count                */
    	g_dmaCTRLPKT2.ELCNT     = 1;                 	/* element count              */
    	g_dmaCTRLPKT2.ELDOFFSET = 0;                	/* element destination offset */
    	g_dmaCTRLPKT2.ELSOFFSET = 0;		          	/* element destination offset */
    	g_dmaCTRLPKT2.FRDOFFSET = 0;		          	/* frame destination offset   */
    	g_dmaCTRLPKT2.FRSOFFSET = 0;                	/* frame destination offset   */
    	g_dmaCTRLPKT2.PORTASGN  = PORTB_READ_PORTA_WRITE;
    	g_dmaCTRLPKT2.RDSIZE    = ACCESS_8_BIT;		    /* read size                  */
    	g_dmaCTRLPKT2.WRSIZE    = ACCESS_8_BIT;	 	    /* write size                 */
    	g_dmaCTRLPKT2.TTYPE     = FRAME_TRANSFER;  	    /* transfer type              */
    	g_dmaCTRLPKT2.ADDMODERD = ADDR_FIXED;        	/* address mode read          */
    	g_dmaCTRLPKT2.ADDMODEWR = ADDR_INC1;      	    /* address mode write         */
    	g_dmaCTRLPKT2.AUTOINIT  = AUTOINIT_OFF;      	/* autoinit                   */
    
    	/*Set control packet for channel 0 and 1*/
    	dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT1);
    	dmaSetCtrlPacket(DMA_CH1, g_dmaCTRLPKT2);
    
    	/*Set dma channel 0 and 1 to trigger on hardware request*/
    	dmaSetChEnable(DMA_CH0, DMA_HW);
    	dmaSetChEnable(DMA_CH1, DMA_HW);
    
    	/*Enable DMA*/
    	dmaEnable();
    
    #if LOOPBACKMODE == 1
    	/*Enable SCI3 Transmit and Receive DMA Request*/
    	sciREG3->SETINT |= SCI_SET_TX_DMA | SCI_SET_RX_DMA | SCI_SET_RX_DMA_ALL;
    
    #else
    	/*Enable SCI3 Transmit and SCI4 Receive DMA Request*/
    	sciREG3->SETINT |= SCI_SET_TX_DMA;
    	sciREG4->SETINT |= SCI_SET_RX_DMA | SCI_SET_RX_DMA_ALL;
    #endif
    
    	while(dmaGetInterruptStatus(DMA_CH1, BTC) != TRUE);
    
    	for(i=0; i<size; i++)
    	{
    		if(RX_DATA[i] != TX_DATA[i])
    		{
    			break;
    		}
    	}
    	if(i<size)
    	{
    		printf("Fail\n");
    	}
    	else
    	{
    		printf("Pass\n");
    	}
    	while(1);
    
    /* USER CODE END */
    }
    
    /* USER CODE BEGIN (4) */
    /* USER CODE END */