Other Parts Discussed in Thread: HALCOGEN
TI的工程师们好,我是一名初学者学生,想知道该芯片在软件上怎么配置进入休眠模式和唤醒模式,有相关的函数接口吗。或者有相应 的demo程序吗?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI的工程师们好,我是一名初学者学生,想知道该芯片在软件上怎么配置进入休眠模式和唤醒模式,有相关的函数接口吗。或者有相应 的demo程序吗?谢谢
您可以下载 HALCoGen,而后在其安装文件夹内可以找到相关例程
https://www.ti.com.cn/tool/cn/HALCOGEN
HALCoGen\v04.07.01\examples
想知道该芯片在软件上怎么配置进入休眠模式和唤醒模式
Hercules MCUs support 3 low-power mode: Doze, Snooze, and Sleep.
To enter the low power mode (sleep mode as example), the following sequence should be followed:
1. Program the flash banks and flash pump fall-back modes to be “sleep”.
2. Disable the clock sources that are not required to be kept active
3. Disable the clock domains that are not required to be kept active.
4. Idle the Cortex-R4F core
The table2-11 lists all the wake-up options: GIO/CAN/SCI interrupts can be used to wake-up the device.
是的,目前没有给出专门的低功耗及唤醒例程
您可以参考我后面的2个链接以及TRM内的2.4.3 Low Power Modes