Part Number: TMS570LC4357
nvsram通过emif连接到tms570lc4357芯片上,怎么配置dma读取nvsram中的数据
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
nvsram通过emif连接到tms570lc4357芯片上,怎么配置dma读取nvsram中的数据
DMA 可以从连接到 EMIF 和 MCU 内部 SRAM 的存储器传输数据字,同时无需任何 CPU 负载。 数据传输由 SW 触发。
以下例子为:将数据从一个存储器位置复制到另一个存储器位置 (EMIF 存储器) :
/** @file HL_sys_main.c
* @brief Application main file
* @date 11-Dec-2018
* @version 04.07.01
*
* This file contains an empty main function,
* which can be used for the application.
*/
/*
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
/* USER CODE BEGIN (1) */
//#include "HL_emif.h"
#include "HL_sys_dma.h"
#include "HL_sys_core.h"
#include "HL_gio.h"
#include "HL_pinmux.h"
#include "HL_esm.h"
/* example data Pattern configuration */
#define E_COUNT 8 /*64, Element count*/
#define F_COUNT 32 /*16, Frame count*/
#define D_SIZE E_COUNT * F_COUNT
void loadDataPattern(uint32 psize, uint32* pptr, uint32 pattern);
#pragma SET_DATA_SECTION(".sharedRAM")
uint32 TXDATA_RAM0[D_SIZE]; /* transmit buffer in sys ram */
uint32 RXDATA_RAM0[D_SIZE]= {0}; /* receive buffer in sys ram */
uint32 TXDATA_RAM1[D_SIZE]; /* transmit buffer in sys ram */
uint32 RXDATA_RAM1[D_SIZE]= {0}; /* receive buffer in sys ram */
g_dmaCTRL g_dmaCTRLPKT1, g_dmaCTRLPKT2; /* dma control packet configuration stack */
#pragma SET_DATA_SECTION()
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
unsigned int Channel0_HBC_Flag;
unsigned int Channel1_HBC_Flag;
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
/* enable IRQ interrupt */
/*clear ESM error*/
uint16 i, j=0;
gioInit();
_enable_IRQ();
Channel0_HBC_Flag = 0;
Channel0_HBC_Flag = 1;
//dmaREG->PTCRL = 0x03 | 0x1 << 3 | 0x1 << 18; /* prority scheme: rotation*/
/* - creating a data chunk in system ram to start with ... */
loadDataPattern(D_SIZE, &TXDATA_RAM0[0], 0x5A5A5A5A);
loadDataPattern(D_SIZE, &TXDATA_RAM1[0], 0x5B5B5B5B);
/* - configuring dma control packets */
g_dmaCTRLPKT1.SADD = (uint32)TXDATA_RAM0; /* source address */
//g_dmaCTRLPKT1.DADD = (uint32)(0x80000000); //(0x08078000); /* destination address; SDRAM */
g_dmaCTRLPKT1.DADD = (uint32)RXDATA_RAM0; //(0x08078000); /* destination address; SDRAM */
g_dmaCTRLPKT1.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT1.FRCNT = F_COUNT; /* frame count */
g_dmaCTRLPKT1.ELCNT = E_COUNT; /* element count */
g_dmaCTRLPKT1.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT1.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT1.PORTASGN = PORTA_READ_PORTA_WRITE;
g_dmaCTRLPKT1.RDSIZE = ACCESS_32_BIT; /* read size */
g_dmaCTRLPKT1.WRSIZE = ACCESS_32_BIT; /* write size */
g_dmaCTRLPKT1.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT1.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT1.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT1.AUTOINIT = AUTOINIT_ON; /* autoinit */
//g_dmaCTRLPKT2.SADD = (uint32)(0x80001000); //0x08076000); /* source address */
g_dmaCTRLPKT2.SADD = (uint32)TXDATA_RAM1; //0x08076000); /* source address */
g_dmaCTRLPKT2.DADD = (uint32)RXDATA_RAM1; /* destination address */
g_dmaCTRLPKT2.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT2.FRCNT = F_COUNT; /* frame count */
g_dmaCTRLPKT2.ELCNT = E_COUNT; /* element count */
g_dmaCTRLPKT2.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.PORTASGN = PORTA_READ_PORTA_WRITE;
g_dmaCTRLPKT2.RDSIZE = ACCESS_32_BIT; /* read size */
g_dmaCTRLPKT2.WRSIZE = ACCESS_32_BIT; /* write size */
g_dmaCTRLPKT2.TTYPE = FRAME_TRANSFER ; /* transfer type */
g_dmaCTRLPKT2.ADDMODERD = ADDR_INC1; /* address mode read */
g_dmaCTRLPKT2.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT2.AUTOINIT = AUTOINIT_ON; /* autoinit */
/* - setting dma control packets */
dmaSetCtrlPacket(DMA_CH1, g_dmaCTRLPKT1); //tx
dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT2); //rx
/* - setting the dma channel to trigger on h/w request */
dmaSetChEnable(DMA_CH1, DMA_SW);
dmaSetChEnable(DMA_CH0, DMA_SW);
/* Enable Block Transfer Complete interrupt for the receive after transfer complete */
dmaEnableInterrupt(DMA_CH0, FTC, DMA_INTA);
dmaEnableInterrupt(DMA_CH1, FTC, DMA_INTA);
dmaEnable();
for(i=1; i<F_COUNT; i++)
{
dmaSetChEnable(DMA_CH1, DMA_SW);
dmaSetChEnable(DMA_CH0, DMA_SW);
j = i;
}
while(1); /* loop forever */
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
/** void loadDataPattern(uint32 psize, uint16* pptr)
*/
void loadDataPattern(uint32 psize, uint32* pptr, uint32 pattern)
{
int i;
for(i=0;i<psize;i++)
{
*(pptr++) = pattern + i;
}
}
/**************************************************************************//**
* DMA Interrupt
*****************************************************************************/
void dmaGroupANotification(dmaInterrupt_t inttype, uint32 channel)
{
/* enter user code between the USER CODE BEGIN and USER CODE END. */
if(channel ==0){
Channel0_HBC_Flag = 1;
}
if(channel == 1){
Channel1_HBC_Flag = 1;
}
}
/* USER CODE END */
希望以上解答对您有所帮助,如有其他问题请随时联系我们。