This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TI TM4C功耗问题



从规格上来看,好像TM4C的工作电流是其他家例如ST,FreeScale的两倍

  • TM4C定位更接近于General的应用,个人认从功耗方面确实无法和定位低功耗的产品进行竞争,但对比通用类的产品应该还是不错的。楼主如果非常在意低功耗推荐考虑TI的MSP430,相信功耗会比您现在看到的功耗更低。

    此外,TI很快会推出TM4L的产品,是针对低功耗应用的M4产品,相信能给楼主更丰富的选择。

  • 待机电流低至 1.6 µA

     运行 RTC 模式低至 1.7 µA
     
    Mode
    Run Mode
    Sleep Mode
    Deep Sleep Mode
    Hibernation (VDD3ON)
    Hibernation
    (RTC)
    Hibernation
     (no RTC)
    Parameter
    IDD
    32 mA
    10 mA
    TBD
    5 μA
    1.7 μA
    1.6 μA
    VDD
    3.3 V
    3.3 V
    3.3 V
    3.3 V
    0 V
    0 V
    VBAT
    N.A.
    N.A.
    N.A.
    3 V
    3 V
    3 V
    System Clock
    40 MHz with PLL
    40 MHz with PLL
    30 kHz
    Off
    Off
    Off
    Core
    Powered On
    Powered On
    Powered On
    Off
    Off
    Off
    Clocked
    Not Clocked
    Not Clocked
    Not Clocked
    Not Clocked
    Not Clocked
    Peripherals
    All On
    All Off
    All Off
    All Off
    All Off
    All Off
    Code
    while{1}
    N.A.
    N.A.
    N.A.
    N.A.
    N.A.
  • 正在测试它的低功耗的,有相关的例程没有呀?

  • 我测试了一下,运行模式下最多不过20mA的。

    我的项目,只要达到10mA就行了的。

  • Vbgood

    M4的hibernation最低可达1.6uA 带RTC可达1.7uA.  至于测试例程, 使用Tivaware下的 ”hibernate“ 即可。