This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于LM4F232H5QD的ADC采样时将采样端电位拉低的问题

Other Parts Discussed in Thread: LM3S8962

大家好:
        我使用的是TI官方的EK-LM4F232H5QD评估板,遇到了以下问题。

        我自己用万用板焊接了一个ADC采样电压反馈电路,在输入端输入一定的电压,在输出端就会输出与之对应的电压值。
        其中LM4F232的引脚PE3(AIN0)外接采样电路的输出端进行AD采样测试,且采样电路的模拟地接到LM4F232板子的GND引脚。
        系统时钟配置时使用了PLL,晶振为16MHz,ADC采样率为125KSps,单端采样,使用的是内部参考电压。


        如果我不用导线将ADC采样电压反馈电路的输出端连接到LM4F232的PE3/AIN0引脚,用万用表测得输出端的电压大小为2.8V;如果我用导线连接到LM4F232的PE3/AIN0引脚,用万用表测得输出端的电压大小降为0.4V,而且从OLED显示的信息来看,ADC采样电压确实是在0.4V左右。
        如果我将LM4F232H5QD的板子换成LM3S8962的板子,就不会出现ADC采样时将采样端电位拉低的现象。
        请问,我接上ADC的采样管脚后,为什么会发生电位拉低的现象?难道是LM4F232板子的ADC内部有拉低电阻?或者M4和M3的内部ADC电路不一样?
        有哪位工程师碰过这种情况的,烦请指点一下,谢谢!
  • 楼主用的是TI的DEMO程序吗?

    换个引脚试试看?

  • Hello,Richard:

          首先感谢您的回复,我看了一下LM4F232H5QD的电路原理图,原来管脚PE3/AIN0,PE,2/AIN1,PE1/AIN2,PE0/AIN3都外接了一个电压跟随器TLV2374PW、一个0欧姆的电阻、一个18欧姆的电阻。如果直接通过接线方式接到这几个管脚上,那么AD输入模拟量不但会进入到芯片的AD转换器,还会构成另外一个回路,从而将电位拉低。

        我将AD采样的管脚改为PD7/AIN4,PD6/AIN5,PD5/AIN6,仍然是多通道采样,单端模式,参考电压选择为外部参考电压3V。这次,我在一个电位器两端加上一个3V的电压(3V由LM4F232板子供给,模拟地已经接回板子了),然后将电位器中间的脚用线接到PD7/AIN4,从OLED显示的信息来看,如果旋转电位器,采样电压在0--3V之间变化。

        但是,这次新的问题又出现了,就是我只是在PD7/AIN4外接一个电位器的脚,按理来说,管脚PD6/AIN5和PD5/AIN6都没有AD输入,采样值应该是0。实际上,采样值不是0。如果管脚PD7/AIN4的采样值为2786mV(用万用表测量是2793mV),则OLED显示:管脚PD6/AIN5的采样值为1000多mV,PD5/AIN6的采样值为400多mV。用万用表测量管脚PD6/AIN5时,则PD6/AIN5的电压值马上降为200多mV。用万用表测量管脚PD5/AIN6时,管脚PD5/AIN6的电压值也是马上降为200多mV。

        我就不明白,为什么管脚PD6/AIN5和PD5/AIN6都没有AD输入时,采样值不是0。同时,用万用表测量管脚PD6/AIN5和PD5/AIN6,对采样值会有影响?还请指教一下,谢谢!!!

  • 输入端要接地或者有确定的输入源,如果什么都不接,电压是浮动的所以采样值是随机值。如果接地时候,应该在0附近,因为会有零漂,但可以软件补偿。

    PD6不接时也有同样问题,可能会受到空间辐射的影响产生随机值。万用表接在上面时,相当于在两点间接了个很大的电阻到地,这时候电压会固定下来

  • Richard,非常感谢你的回复!Good  luck!

  • EK-LM4F120XL Launchpad中,

    我分别用

    AIN0(PE3口)采样1.3V电压

    AIN1(PE2口)采样0.65V电压,

    AIN8(PE5口)采样1.95V电压,

    AIN9(PE4口)采样2.6V电压,

    假如以3.0V作为参考电压,那么在数据寄存器中采样结果应该是:

    1775,对应1.3V电压

    888,对应采样0.65V电压,

    2659,对应采样1.95V电压,

    3563,对应采样2.6V电压,

    但是实际结果是:

    AIN0:1645,根据1.3*4096/1645=3.23,参考电压为3.23V,

    AIN1:1005,根据0.65*4096/1005=2.65,参考电压为2.65V,

    AIN8:2175,根据1.95*4096/2175=3.76,参考电压为3.67V,

    AIN9:2765,根据2.61*4096/2765=3.87,参考电压为3.87V,

    如上,每次的结果都不一样。这是为什么呢?(如果参考电压假定为3.3V,结果也是类似的)

    我的源程序如下(采样时只要修改相应的端口就可以了):


    #include"inc/hw_ints.h"
    #include"inc/hw_types.h"
    #include"inc/hw_memmap.h"

    #include"driverlib/sysctl.h"
    #include"driverlib/interrupt.h"
    #include"driverlib/adc.h"
    #include"driverlib/gpio.h"


    unsigned char adc_endflag=0;


    void enable_adc_pin()
    {

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
    GPIOPinTypeADC(GPIO_PORTE_BASE,GPIO_PIN_2);

    }

    void config_adc()
    {
    SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
    SysCtlADCSpeedSet(SYSCTL_ADCSPEED_125KSPS);

    ADCSequenceConfigure(ADC0_BASE, 0, ADC_TRIGGER_PROCESSOR, 0);
    ADCSequenceStepConfigure(ADC0_BASE,0,0,ADC_CTL_CH1|ADC_CTL_END|ADC_CTL_IE);
    ADCSequenceEnable(ADC0_BASE, 0);

    ADCIntEnable(ADC0_BASE,0);
    IntEnable(INT_ADC0);
    IntMasterEnable();

    }

    unsigned long start_adc_sample()
    {
    unsigned long ulvalue;

    ADCProcessorTrigger(ADC0_BASE,0);
    while(adc_endflag==0);
    adc_endflag=0;


    ADCSequenceDataGet(ADC0_BASE,0,&ulvalue);

    return(ulvalue);

    }
    void main()
    {

    //SysCtlClockSet(SYSCTL_SYSDIV_4|SYSCTL_USE_PLL|
    // SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);


    SysCtlClockSet(SYSCTL_SYSDIV_10 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN |
    SYSCTL_XTAL_16MHZ);

    unsigned int ulva[40]={0};
    unsigned char i=0;
    enable_adc_pin();
    config_adc();


    while(1)
    {
    ulva[i]=start_adc_sample();
    if(ulva[i]>4000)
    ulva[i]=0;
    i+=1;
    if(i==40)
    i=0;
    SysCtlDelay(20000);

    }


    }


    void adc_int_isr()
    {
    ADCIntClear(ADC0_BASE,0);
    adc_endflag=1;

    }