This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: How to change DLC when sending,

Part Number: TMS570LC4357

How to change DLC when sending,如何发送可变字节长度的报文

I modified the DLC value in the cantransmit function, but it still failed.  我在canTransmit函数中修改DLC的值但还是不行

有没有参考的流程,手册我已经看了很多次了还是不太明白。

  • 你好,问题已经收到,我需要向其他工程师咨询一下之后再回复你,还请耐心等待。

  • 我也想知道如何读取接收到报文的DLC值

  • 可以在将数据从 IFx 寄存器传输到 DCAN 消息 RAM 或邮箱之前更新 DLC。 HAL 代码没有更新 DLC 的 API,但可以编写自己的 API。 例如:

    Fullscreen
    1
    2
    3
    4
    5
    6
    7
    8
    9
    10
    11
    12
    13
    14
    15
    16
    17
    18
    19
    20
    21
    void canUpdateDLC(canBASE_t *node, uint32 messageBox, uint8 msgBoxDLC)
    {
    /** - Wait until IF2 is ready for use */
    while ((node->IF2STAT & 0x80U) ==0x80U)
    {
    } /* Wait */
    node->IF2CMD = 0x90U;
    node->IF2MCTL &= ~(uint32)(0xFU);
    node->IF2MCTL |= (uint32)(msgBoxDLC & 0xFU);
    node->IF2NO = (uint8) messageBox;
    /** - Wait until data are copied into IF2 */
    while ((node->IF2STAT & 0x80U) ==0x80U)
    {
    } /* Wait */
    XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

    消息对象的DLC必须定义为与其他节点具有相同标识符的相应对象中的值相同。

  • //可以把这个程序添加在Transmit函数里面吗?

    uint32 canTransmit(canBASE_t *node, uint32 messageBox, const uint8 * data,uint8 msgBoxDLC)
    {
    uint32 i;
    uint32 success = 0U;
    uint32 regIndex = (messageBox - 1U) >> 5U;
    uint32 bitIndex = 1U << ((messageBox - 1U) & 0x1FU);


    /* USER CODE BEGIN (7) */     //添加在这里

    /** - Wait until IF2 is ready for use */
    while ((node->IF2STAT & 0x80U) ==0x80U)
    {
    } /* Wait */

    node->IF2CMD = 0x90U;

    node->IF2MCTL &= ~(uint32)(0xFU);

    node->IF2MCTL |= (uint32)(msgBoxDLC & 0xFU);

    node->IF2NO = (uint8) messageBox;

    /** - Wait until data are copied into IF2 */
    while ((node->IF2STAT & 0x80U) ==0x80U)
    {
    } /* Wait */

    /* USER CODE END */

    /** - Check for pending message:
    * - pending message, return 0
    * - no pending message, start new transmission
    */

    if ((node->TXRQx[regIndex] & bitIndex) != 0U)
    {
    success = 0U;
    }

    else
    {
    /** - Wait until IF1 is ready for use */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
    while ((node->IF1STAT & 0x80U) ==0x80U)
    {
    } /* Wait */

    /** - Configure IF1 for
    * - Message direction - Write
    * - Data Update
    * - Start Transmission
    */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */


    /** - Copy TX data into IF1 */
    for (i = 0U; i < msgBoxDLC; i++)                 //这里循环条件改成DLC
    {
    #if ((__little_endian__ == 1) || (__LITTLE_ENDIAN__ == 1))
    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
    node->IF1DATx[i] = *data;
    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
    data++;
    #else
    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
    node->IF1DATx[s_canByteOrder[i]] = *data;
    /*SAFETYMCUSW 45 D MR:21.1 <APPROVED> "Valid non NULL input parameters are only allowed in this driver" */
    data++;
    #endif
    }

    /** - Copy TX data into message box */
    /*SAFETYMCUSW 93 S MR: 6.1,6.2,10.1,10.2,10.3,10.4 <APPROVED> "LDRA Tool issue" */
    node->IF1NO = (uint8) messageBox;

    success = 1U;
    }
    /** @note The function canInit has to be called before this function can be used.\n
    * The user is responsible to initialize the message box.
    */

    /* USER CODE BEGIN (8) */
    /* USER CODE END */

    return success;
    }

  • 接收到的报文怎么读取DLC

  • 收到,我会尽快帮你反馈。

  • 使用canUpdateID函数更新ID后,发送的数据帧变成远程帧了,我不知道原因

  • 这是新问题?新问题的话还请麻烦新开一个帖子,都放一起会乱

  • 客气了,之前的问题应该会在明天回复你。

  • 1、是的,可以将新 ID、DLC 添加到传输 API。

    /** - Copy TX data into IF1 */
    for (i = 0U; i < msgBoxDLC; i++)                 //这里循环条件改成DLC

    这里不必将 8 更改为 msgBoxDLC。 无论 DLC 有多小,八字节数据都会从 IFx 数据寄存器(A 和 B)传输到消息 RAM。

    2、DLC 是消息控制寄存器的一部分。 您需要设置 CMD 寄存器的 CONTROL 位和 CMD 寄存器的 CLEAR W/R 位,以便将 DLC 从 Message RAM 传输到 Fx 寄存器:

    canGetData(0 API include this portion:

    /** - Configure IF2 for
    * - Message direction - Read
    * - Data Read
    * - Clears NewDat bit in the message object.
    */
    node->IF2CMD = 0x17U;

    /** - Copy data into IF2 */
    /*SAFETYMCUSW 93 S MR: 6.1,6.2,10.1,10.2,10.3,10.4 <APPROVED> "LDRA Tool issue" */
    node->IF2NO = (uint8) messageBox;

    /** - Wait until data are copied into IF2 */
    /*SAFETYMCUSW 28 D MR:NA <APPROVED> "Potentially infinite loop found - Hardware Status check for execution sequence" */
    while ((node->IF2STAT & 0x80U) ==0x80U)
    {
    } /* Wait */

    /** - Get number of received bytes */
    size = node->IF2MCTL & 0xFU;
    if(size > 0x8U)
    {
    size = 0x8U;
    }
    /** - Copy RX data into destination buffer */