Part Number: AM2732
在SDK/example/cbuff工程上做了一定修改,使之可以一直用LVDS发送数据,但是用示波器测量LVDS接口,也就是EVM板上的J7,发现没有任何信号输出。手上没有DCA采数板,无法进行其他验证方式。
问题1:是不是cbuff工程成功运行,理论上就会有LVDS信号输出?
问题2:如果不是,我还需要进行哪些步骤?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2732
在SDK/example/cbuff工程上做了一定修改,使之可以一直用LVDS发送数据,但是用示波器测量LVDS接口,也就是EVM板上的J7,发现没有任何信号输出。手上没有DCA采数板,无法进行其他验证方式。
问题1:是不是cbuff工程成功运行,理论上就会有LVDS信号输出?
问题2:如果不是,我还需要进行哪些步骤?
请问做了什么修改?没做修改前,有LVDS输出么?请参考下面对例程的说明。
https://software-dl.ti.com/mcu-plus-sdk/esd/AM273X/08_02_00_26/exports/docs/api_guide_am273x/EXAMPLES_DRIVERS_CBUFF_SW_TRIGGER.html
主要修改了cbuff的传输次数,原代码中cbuff只传输一次,然后就关闭了。我将CBUFF_activateSession函数和CBUFF_deactivateSession函数放在死循环中,这样am2732就可以一直让cbuff发送数据了。具体修改情况如插入代码,在cbuff_sw_trigger.c文件270行之前(也就是插入代码的第一行)只加入了gCBUFFSwTriggerFrameDoneCounter_last变量的定义,其他无修改,其他文件也无修改。修改的地方是1.加入了gCBUFFSwTriggerFrameDoneCounter_last变量,通过它和gCBUFFSwTriggerFrameDoneCounter是否相等判断本次传输是否完成。2.屏蔽了后面的cbuff_close等程序结束关闭代码。
/* Create the Session: */
sessionHandle = CBUFF_createSession (cbuffHandle, &sessionCfg, &errCode);
if (sessionHandle == NULL)
{
DebugP_log ("Error: Unable to create the session [Error code %d]\r\n", errCode);
}
while(1)
{
/* Activate the session: */
if (CBUFF_activateSession (sessionHandle, &errCode) < 0)
{
DebugP_log ("Error: Unable to activate the session [Error code %d]\r\n", errCode);
}
while (gCBUFFSwTriggerFrameDoneCounter == gCBUFFSwTriggerFrameDoneCounter_last)
{
DebugP_log("waiting for frameDone interrupt : %d\r\n", gCBUFFSwTriggerFrameDoneCounter);
ClockP_usleep(10 * 1000);
}
DebugP_log("Received frameDone interrupt : %d\r\n", gCBUFFSwTriggerFrameDoneCounter);
gCBUFFSwTriggerFrameDoneCounter_last = gCBUFFSwTriggerFrameDoneCounter;
/* Deactivate the session: */
if (CBUFF_deactivateSession (sessionHandle, &errCode) < 0)
{
DebugP_log ("Error: Unable to deactivate the session [Error code %d]\r\n", errCode);
}
}
// /* Delete the session: */
// if (CBUFF_close (sessionHandle, &errCode) < 0)
// {
// DebugP_log ("Error: Unable to delete the session [Error code %d]\r\n", errCode);
// }
// if(testStatus == SystemP_SUCCESS)
// {
// DebugP_log("[CBUFF] SW Trigger Test Completed!!\r\n");
// DebugP_log("All tests have passed!!\r\n");
// }
// else
// {
// DebugP_log("Some tests have failed!!\r\n");
// }
// Board_driversClose();
// Drivers_close();
// return;