Part Number: AM2634
大家好:
我方目前使用AM263X-LP开发板,在测试外部Flash启动,我在烧录时将外部Flash全部擦除,未写入新的文件。重新上电后发现不能正常Debug,请问在这是什么原因?
我的引导模式选择为0101(QSPI (1S) - 单路读取 UART 回退模式),开发板上电后串口会有如下信息显示:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请看一下如果直接设置成uart boot模式,是否能进入uart boot模式?具体步骤可以看一下下面文档。
https://software-dl.ti.com/mcu-plus-sdk/esd/AM263X/08_03_01_06/exports/docs/api_guide_am263x/TOOLS_BOOT.html#UART_BOOTLOADER_PYTHON_SCRIPT
请问按照上面文档中的步骤配置后,串口有打印cccc吗?
请看下面工程师的回复。
The AM263x-LP has default SBL NULL present on the flash. This secondary bootloader is loaded by ROM after identifying a valid x509 certificate. The SBL_NULL boots all the cores and executes WFI. This allows users to connects the debugger to any core and program an application via CCS.
As you have removed the SBL, the ROM is not able to recognize any valid x509 certificate, the cores are not correctly initialized. This is the reason, why you are not able to connect the debugger properly. This is also the reason you are seeing XMODEM prints from ROM with "C" because the X509 parsing has failed in QSPI and ROM could not boot any image hence it is waiting for a valid application via UART.
I suggest you to add a valid SBL (preferably SBL_NULL) if you intend to load the application via CCS.