This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LX4F232H5QC 与TM4C1233E6PZ 在CAN上的区别

Other Parts Discussed in Thread: TM4C1233E6PZ

本人有两块板子,一个芯片为LX4F232H5QC,一块为TM4C1233E6PZ,同样的程序,配置CAN1的时候LX4F232H5QC的板子上就可以正常运行,、

而在TM4C1233E6PZ这个板子在CANInit(CAN1_BASE);就出现了异常,无法使用。想请教一下原因是什么?

代码如下:

ROM_FPULazyStackingEnable();
ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTH_BASE, GPIO_PIN_2);
GPIOPinWrite(GPIO_PORTH_BASE, GPIO_PIN_2, 0x04);

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_3);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, 0x08);

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_4);
GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_4, 0x10);

SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN1);
GPIOPinConfigure(GPIO_PA0_CAN1RX);
GPIOPinConfigure(GPIO_PA1_CAN1TX);

GPIOPinTypeCAN(GPIO_PORTA_BASE,GPIO_PIN_0|GPIO_PIN_1);
CANInit(CAN1_BASE);
CANBitRateSet(CAN1_BASE,SysCtlClockGet(),500000);

CANEnable(CAN1_BASE);
IntEnable(INT_CAN1);
CANIntEnable(CAN1_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);