This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【TI eStore最热销产品荐】传感器集线器 BoosterPack(BOOSTXL-SENSHUB)



描述

TI 传感器集线器 BoosterPack(BOOSTXL-SENSHUB)是一款专为 Tiva™ C 系列 TM4C123G LaunchPad 开发板而设计的附加板。这款基于 TI Tiva 平台的传感器集线器 BoosterPack 可以用来评估基于 ARM® Cortex™-M4 TM4C 设备的传感器融合应用,展示 M4 架构在数理及算法方面的特性。

特性

Seven on-board sensor functions, including:

  • InvenSense MPU-9150: 9-axis MEMS motion tracking
    • 3-axis gyro
    • 3-axis accelerometer
    • 3-axis compass
  • Bosch Sensortec BMP180 pressure sensor
  • Sensirion SHT21 humidity and ambient temperature sensor
  • Intersil ISL29023 ambient and infrared light sensor
  • TI's TMP006 non-contact infrared temperature sensor

Uses BoosterPack XL connection standard:

  • Two pairs of 10-pin headers provide standard LaunchPad interface
  • Primary header (outer row) compatible with other TI MCU LaunchPads
  • Secondary header (inner row) offers additional Tiva C Series-based expansion signals
  • 2× user input buttons and LEDs
  • TI’s wireless evaluation module (EM) interface connection

The Sensor Hub BoosterPack also features the Air Mouse (PC HID) example application to demonstrate sensor fusion technology.

The Sensor Hub BoosterPack is supported by TivaWare™ for C Series Driver Library and is compatible with these toolchains:

  • Code Composer Studio™ IDE
  • Keil™ RealView®
  • IAR Systems Embedded Workbench®
  • Mentor Embedded Sourcery CodeBench™