Part Number: AM2434
按现在情况,请问AM243x芯片,2022年底量产可能信有多大?何时会量产?
另外,AM2434芯片,DSMC控制R5的bootloader启动,查找主启动需要3分钟,没有才进入第二启动,这太不合理了,贵公司是否意识到这个问题,考虑过用户感受吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
查找主启动需要3分钟,没有才进入第二启动
请问主启动是什么模式? 第二启动是指secondary bootloader么?3分钟是怎么测量得到的?
主启动是串口,第二启动是指Backup Boot,使用的是QSPI,要进入Backup Boot启动,必须要等3分钟,这样启动设置根本不合理
请看下面e2e工程师的回复。
This does not block boot for 3 minutes. Please check the Note below the flow chart in the TRM and extract here:
DMSC ROM sets up a 3-minute watchdog timer (MCU_RTI0) timeout. During this time, the MCU boot needs to get completed, otherwise a WDT reset will occur. Once the R5 image is loaded (SBL/SPL), DMSC ROM will restart the watchdog timer for additional 3 minutes upon entering the R5 SBL. The customer-provided MCU image needs to load and install the TI-provided SYSFW image into the DMSC, which will manage the watchdog timer during run time.
另外,请AM243x量产,在什么时间
这个问题还在等e2e工程师回复。