This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335X boot sequence

请问一下,AM335X boot sequence 设置里面SYSBOOT[15:0] 所对应的pin?谢谢!

  • AM335X的BOOT 有多种接口和顺序可以选用,SYSBOOT寄存器的[4:0]就是用来配置BOOT所使用的接口和顺序的。

    以SYSBOOT[4:0] = 00001b为例子,表示可以通过UART0(1), XIP w(2), MMC0(3), SPI0(4)接口boot. ()中表示的是BOOT顺序。

    上电后,AM335X会首先检测UART0接口,也就是默认的UART0_RXD_GPIO1[10]和UART0_TXD_GPIO1[11].

    更具体的描述你要参见数据手册的SYSBOOT寄存器描述。