This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123G PF0管脚输出PWM问题



#include <stdbool.h>

#include <stdint.h>

#include "inc/hw_ints.h"

#include "inc/hw_memmap.h"

#include "driverlib/gpio.h"

#include "driverlib/interrupt.h"

#include "driverlib/pin_map.h"

#include "driverlib/pwm.h"

#include "driverlib/sysctl.h"

#include "driverlib/uart.h"

#include "utils/uartstdio.h"

 

//*****************************************************************************

//主程序

int

main(void)

{

 

    //

    // 设置系统时钟16M

    SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN |

                   SYSCTL_XTAL_16MHZ);

 

    //

    // PWM不分频

    //

    SysCtlPWMClockSet(SYSCTL_PWMDIV_1);

 

 

    //使能M1PWM外设

 

 

    SysCtlPeripheralEnable(SYSCTL_PERIPH_PWM1);

 

 

    //使能M1PWM用到的PF,和RESET对应的PB

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);//使能B端口,PB2、PB3分别对应RESET_AB,RESET_CD

    GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_2|GPIO_PIN_3);//配置2,3管脚为输出

 

    //配置PF0,PF1分别为M1PWM4,M1PWM5

    GPIOPinConfigure(GPIO_PF0_M1PWM4);

    GPIOPinConfigure(GPIO_PF1_M1PWM5);

 

 

    // 配置PF0,PF1为PWM的输出管脚

    GPIOPinTypePWM(GPIO_PORTF_BASE, GPIO_PIN_0|GPIO_PIN_1);

 

    //

    // Configure the PWM1 to count down without synchronization.

    //配置GEN2递减计数模式不同步模式

    PWMGenConfigure(PWM1_BASE, PWM_GEN_2,

                    PWM_GEN_MODE_DOWN | PWM_GEN_MODE_NO_SYNC);

 

    //

    // Set the PWM period to 250Hz.  To calculate the appropriate parameter

    // use the following equation: N = (1 / f) * SysClk.  Where N is the

    // function parameter, f is the desired frequency, and SysClk is the

    // system clock frequency.

    // In this case you get: (1 / 250Hz) * 16MHz = 64000 cycles.  Note that

    // the maximum period you can set is 2^16.

    //设置PWM周期

 

    PWMGenPeriodSet(PWM1_BASE, PWM_GEN_2,100);

 

    //

    // For this example the PWM0 duty cycle will be variable.  The duty cycle

    // will start at 0.1% (0.01 * 64000 cycles = 640 cycles) and will increase

    // to 75% (0.5 * 64000 cycles = 32000 cycles).  After a duty cycle of 75%

    // is reached, it is reset to 0.1%.  This dynamic adjustment of the pulse

    // width is done in the PWM0 load interrupt, which increases the duty

    // cycle by 0.1% everytime the reload interrupt is received.

    //设置PWM占空比

    PWMPulseWidthSet(PWM1_BASE, PWM_OUT_4, 100/2);

    PWMPulseWidthSet(PWM1_BASE, PWM_OUT_5, 100/2);

 

    //使能PWM输出状态

    PWMOutputState(PWM1_BASE, PWM_OUT_4_BIT| PWM_OUT_5_BIT, true);

    GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_2, 0x1<<2);//H2管脚置高  对应RESETAB

    GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_3, 0x1<<3);//H3管脚置高 对应RESETCD

 

    //

    // 使能PWM发生器

    PWMGenEnable(PWM1_BASE, PWM_GEN_2);

 

 

    //循环等待响应

    while(1)

    {

 

    }

}

PF1能输出PWM,PF0不能输出PWM