M4处理器TM4C123GH6PGE的AD Vref+和Vref-之间选用外部的参考电源3.0V,但是AD的pin输入可能达到3.3V,这样会不会损坏芯片?因为如果超过了3V,AD就认为是满量程,即大于等于3.0V就认为是最大量程。手册上说AD的输入最大在Vref+,超过但是没有超3.3V(即VDD和VDDA)会不会有问题?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
M4处理器TM4C123GH6PGE的AD Vref+和Vref-之间选用外部的参考电源3.0V,但是AD的pin输入可能达到3.3V,这样会不会损坏芯片?因为如果超过了3V,AD就认为是满量程,即大于等于3.0V就认为是最大量程。手册上说AD的输入最大在Vref+,超过但是没有超3.3V(即VDD和VDDA)会不会有问题?谢谢!
楼主,
手册上写的是最大输入在Vref+,也就是说如果模拟输入超过了这个范围,在实际使用过程中也许不会出现问题,但是不能保证没有问题。所以建议还是按照手册上的要求,调整模拟输入范围或者参考电平。