This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TM4c123gxl上的输入捕获中断,看了前面的几个帖子,改了配置还是进不去中断,求指点!!!



int main(void)
{

    //sys config    
    SysCtlClockSet(SYSCTL_SYSDIV_4|SYSCTL_USE_PLL
                      |SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ);

    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
    SysCtlDelay(200);
    
    //GPIO config
    GPIOPinTypeTimer(GPIO_PORTB_BASE, GPIO_PIN_7);
    GPIOPinConfigure(GPIO_PB7_T0CCP1);
    GPIODirModeSet(GPIO_PORTB_BASE,GPIO_PIN_7,GPIO_DIR_MODE_IN);

    //Timer config
    TimerConfigure(TIMER0_BASE, TIMER_CFG_SPLIT_PAIR | TIMER_CFG_B_CAP_TIME_UP);
    TimerControlEvent(TIMER0_BASE, TIMER_B, TIMER_EVENT_POS_EDGE);

    //Int config
    IntEnable(INT_TIMER0B);
    TimerIntEnable(TIMER0_BASE, TIMER_CAPB_EVENT);
    IntMasterEnable();
    TimerEnable(TIMER0_BASE, TIMER_B);
    
    while(1);
}
void Timer0B_Int_Handler()
{
    TimerIntClear(TIMER0_BASE, TIMER_CAPB_EVENT);
    GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_2, GPIO_PIN_2);
    GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, GPIO_PIN_3);
    SysCtlDelay(SysCtlClockGet() /10);
}

已经在startup_ccs.c中添加声明了中断函数。