This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PMI 的烧写问题

Other Parts Discussed in Thread: TM4C123GH6PM

刚学这个,

我的环境是:CCS5.4.0

这是我写的代码:

#include <stdint.h>
#include <stdbool.h>
#include "inc/tm4c123gh6pm.h"
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/gpio.h"

void main(void)
{
volatile uint32_t ulLoop = 0;
volatile uint32_t ui8PinData = 2;

/*------------------------------------------------------------------------*/
//设置系统时钟:(400MHZ /2)/5 = 40 MHZ
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
/*------------------------------------------------------------------------*/


/*------------------------------------------------------------------------*/
//使能GPIOF端口
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);

//设置GPIOF中PF3、PF2、PF1引脚为输出(挂在APB总线)
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
//设置GPIOF中PF3、PF2、PF1引脚为输出(挂在AHB总线)
//GPIOPinTypeGPIOOutput(GPIO_PORTF_AHB_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);

//设置GPIOF中PF3、PF2、PF1引脚为输出为8MA, 推挽输出(基址,要操作的位,电流选择,模式选择【】)
GPIOPadConfigSet(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);

/*------------------------------------------------------------------------*/

while(1)
{
//红灯亮
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,0x02);

//延时
SysCtlDelay(2000000);

//蓝灯亮
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,0x04);

//延时
SysCtlDelay(2000000);

//绿灯亮
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3,0x08);

//延时1ms*1000
SysCtlDelay(SysCtlClockGet()/3000*1000);
}
}

问题在于:调试模式下,点击运行确实可以正常运行;

但是,当我用LM Flash Programmer将.bin文件烧写进去时,上电/复位后毫无反应。

另:TIVAWAVE里的例子我烧写了一个进去,可以正常运行。现在很困惑我到底是哪里错了?