This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs 报错 unresolved symbol remain



/*
 * main.c
 */
//display the frequency and amplitude
#ifndef  __LCD_MODULE_H__
#define  __LCD_MODULE_H__
#endif

#ifndef TARGET_IS_BLIZZARD_RB1
#define TARGET_IS_BLIZZARD_RB1
#endif

#ifndef PART_TM4C123GH6PM
#define PART_TM4C123GH6PM
#endif

#include<stdint.h>
#include<stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include"driverlib/sysctl.h"
#include "driverlib/timer.h"
#include"driverlib/rom.h"
#include "inc/tm4c123gh6pge.h"
#include "LCD_module.h"

extern uint8_t LCD_ASCII[127][16];
float Frequency=12345.12,Amplitude=0;

void display(void)
{   uint8_t i;
	uint8_t temp_frequency[7];
   // uint8_t temp_amplitude[4];
	LCD_string_16x8(1,1,"Frequency:");

	//get the value of the array
	temp_frequency[0]=(int)Frequency/10000;//10k
	temp_frequency[1]=((int)Frequency%10000)/1000;//1k
	temp_frequency[2]=((int)Frequency/100)%10;//100
	temp_frequency[3]=((int)Frequency/10)%10;//10
	temp_frequency[4]=(int)Frequency%10;//1
	temp_frequency[5]=((int)Frequency*10)%10;//0.1
	temp_frequency[6]=((int)Frequency*100)%10;//0.01

	//display the frequency
	
	for(i=1;i<=5;i++)
		{
		if(temp_frequency[i]!=0)
			LCD_char_16x8(2,i+2,temp_frequency+i);
		}
	//display "."
	LCD_char_16x8(2,8,LCD_ASCII[46]);
	//display the point
	for(i=1;i<=2;i++)
		LCD_char_16x8(2,i+8,temp_frequency+i+4);
	//display "Hz"
	LCD_string_16x8(2,10,"Hz");
}