表现是这样。用CCS5.5和大学计划的license。用luanchpad下载。同一个程序。下载程序有时候可以成功有时候不可以成功。对于不可以成功的程序在在线调试的时候发现是在外设初始化的时候进入了FaultISR。Launchpad肯定没问题。换了三四块试了,新的旧的,stellaris的也用过。
程序包含了adc0,timer0,timer1,udma。中断包含了ADC和timer1的中断。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
表现是这样。用CCS5.5和大学计划的license。用luanchpad下载。同一个程序。下载程序有时候可以成功有时候不可以成功。对于不可以成功的程序在在线调试的时候发现是在外设初始化的时候进入了FaultISR。Launchpad肯定没问题。换了三四块试了,新的旧的,stellaris的也用过。
程序包含了adc0,timer0,timer1,udma。中断包含了ADC和timer1的中断。
void ADC0withDMA_init(void)
{
unsigned int uIdx;
for(uIdx = 0; uIdx < ADC_DSTBUF_SIZE; uIdx++)
{
g_ulAdcBuf[uIdx] = 0;
}
SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);//此处顺序必须不得更改。
// Enable GPIO for ADC
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_3);// Enable pin PE3 for ADC AIN0
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_2);// Enable pin PE2 for ADC AIN1
GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_1);// Enable pin PE1 for ADC AIN2
GPIOPinTypeADC(GPIO_PORTD_BASE, GPIO_PIN_3);// Enable pin PD3 for ADC AIN4
//ADCSequenceDisable(ADC0_BASE, 1);
//SysCtlADCSpeedSet(SYSCTL_ADCSPEED_250KSPS);
ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_TIMER, 0);
ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_CH0);
ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_CH1| ADC_CTL_IE );
ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_CH2);
ADCSequenceStepConfigure(ADC0_BASE, 1, 3, ADC_CTL_CH4| ADC_CTL_IE |ADC_CTL_END);
//ADC0_CC_R=0x01;
ADCSequenceOverflowClear(ADC0_BASE,1);//不知道为什么会触发overflow中断
ADCIntClear(ADC0_BASE, 1);
ADCIntEnableEx(ADC0_BASE,ADC_INT_DMA_SS1);
ADCIntRegister(ADC0_BASE,1,ADC0_ISR);
SysCtlPeripheralEnable(SYSCTL_PERIPH_UDMA);
uDMAEnable();
uDMAControlBaseSet(sDMAControlTable);
uDMAChannelAttributeEnable(UDMA_CHANNEL_ADC1 | UDMA_PRI_SELECT,UDMA_ATTR_USEBURST|UDMA_ATTR_HIGH_PRIORITY);
uDMAChannelControlSet(UDMA_CHANNEL_ADC1 | UDMA_PRI_SELECT, UDMA_SIZE_32 | UDMA_SRC_INC_NONE |UDMA_DST_INC_32 | UDMA_ARB_2);
uDMAChannelTransferSet(UDMA_CHANNEL_ADC1 | UDMA_PRI_SELECT,UDMA_MODE_BASIC,(void *)(ADC0_BASE+ADC_O_SSFIFO0 - ADC_O_SSMUX0+ADC_O_SSMUX1),g_ulAdcBuf, ADC_DSTBUF_SIZE/2);
uDMAChannelEnable(UDMA_CHANNEL_ADC1);
ADCSequenceDMAEnable(ADC0_BASE,1);
ADCSequenceEnable(ADC0_BASE, 1);
}
void TimerforAdc_init(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER0));
TimerConfigure(TIMER0_BASE, TIMER_CFG_SPLIT_PAIR|TIMER_CFG_A_PERIODIC_UP);
TimerLoadSet(TIMER0_BASE, TIMER_A, 10000);//period
//TimerPrescaleSet(TIMER0_BASE,TIMER_A,2);
TimerControlTrigger(TIMER0_BASE, TIMER_A, true);//trigger ADC with TIMER
TimerControlStall(TIMER0_BASE, TIMER_A, true);//调试时暂停计数(必要!)
//SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//GPIOPinConfigure(GPIO_PB6_T0CCP0);
//GPIOPinTypeTimer(GPIO_PORTB_BASE, GPIO_PIN_6);
//TimerMatchSet(TIMER0_BASE, TIMER_A,TimerLoadGet(TIMER0_BASE, TIMER_A) / 3);
TimerEnable(TIMER0_BASE, TIMER_A);
//TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC_UP);
}
void Timerforscreen_init(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER1));
//while(!SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER1));
TimerConfigure(TIMER1_BASE, TIMER_CFG_SPLIT_PAIR|TIMER_CFG_A_PERIODIC);
TimerLoadSet(TIMER1_BASE, TIMER_A, 60000);//period
TimerPrescaleSet(TIMER1_BASE,TIMER_A,255);
//TimerControlStall(TIMER0_BASE, TIMER_B, true);//调试时暂停计数(必要!)
unsigned long ulStatus;
ulStatus = TimerIntStatus(TIMER1_BASE,true);
TimerIntClear(TIMER1_BASE,ulStatus);
TimerIntRegister(TIMER1_BASE,TIMER_A,Timer1A_ISR);
TimerIntEnable(TIMER1_BASE,TIMER_TIMA_TIMEOUT);
IntEnable(INT_TIMER1A);
//SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
//GPIOPinConfigure(GPIO_PB7_T0CCP1);
//GPIOPinTypeTimer(GPIO_PORTB_BASE, GPIO_PIN_7);
//TimerMatchSet(TIMER0_BASE, TIMER_B,TimerLoadGet(TIMER0_BASE, TIMER_B) / 3);
//TimerIntClear(TIMER1_BASE,TIMER_TIMA_TIMEOUT);
TimerEnable(TIMER1_BASE, TIMER_A);
}
主要就是这三个初始化嫌疑比较大。现在下载程序都要下载两遍才能用。