Other Parts Discussed in Thread: EK-TM4C123GXL
配置UART0为接收到数据产生中断存在数组里,但是每次都会卡死在FaultISR函数里面?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: EK-TM4C123GXL
配置UART0为接收到数据产生中断存在数组里,但是每次都会卡死在FaultISR函数里面?
对照例程看一下:
C:\ti\TivaWare_C_Series-2.1.0.12573\examples\boards\ek-tm4c123gxl\uart_echo
或者把源码贴上来一起看看。
仿真,然后程序停在FaultISR的时候看一下link寄存器,这里保存了跳转前的地址。
其实也不用这么复杂,理顺程序后把问题解决了就行了
源码如下
//*****************************************************************************
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
uint8_t RxData[9]={0};
uint8_t UartRxDatFlag = false;
uint8_t UartTxIntEnFlag = false;
uint16_t UartTxLen = 0;
uint16_t UartTxIndex = 0;
//*****************************************************************************
//
//! \addtogroup uart_examples_list
//! <h1>UART Polled I/O (uart_polled)</h1>
//!
//! This example shows how to set up the UART and use polled I/O methods
//! for transmitting and receiving UART data. The example receives characters
//! from UART0 and retransmits the same character using UART0. It can be
//! tested by using a serial terminal program on a host computer. This
//! example will echo every character that is type until the return/enter key
//! is pressed.
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - UART0 peripheral
//! - GPIO Port A peripheral (for UART0 pins)
//! - UART0RX - PA0
//! - UART0TX - PA1
//
//*****************************************************************************
void UART0IntHandler(void)
{
uint32_t ui32Status = 0;
//获取中断状态
ui32Status = UARTIntStatus(UART0_BASE, true);
//清除中断标志
ROM_UARTIntClear(UART0_BASE, ui32Status);
RxData[UartTxLen ++]=UARTCharGet(UART0_BASE);
if(UartTxLen ==9)
{
UartTxLen =0;
for(UartTxIndex=0;UartTxIndex<9;UartTxIndex++)
{
UARTCharPutNonBlocking(UART0_BASE,RxData[UartTxIndex]);
// RxData[UartTxIndex]=0;
}
// UARTprintf("\n");
}
}
//*****************************************************************************
//
// Configure the UART and perform reads and writes using polled I/O.
//
//*****************************************************************************
void INT_UART(void)
{
// Enable the peripherals used by this example.
// The UART itself needs to be enabled, as well as the GPIO port
// containing the pins that will be used.
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
// Configure the GPIO pin muxing for the UART function.
// This is only necessary if your part supports GPIO pin function muxing.
// Study the data sheet to see which functions are allocated per pin.
// TODO: change this to select the port/pin you are using
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
//
// Since GPIO A0 and A1 are used for the UART function, they must be
// configured for use as a peripheral function (instead of GPIO).
// TODO: change this to match the port/pin you are using
//
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Configure the UART for 115,200, 8-N-1 operation.
// This function uses SysCtlClockGet() to get the system clock
// frequency. This could be also be a variable or hard coded value
// instead of a function call.
//
/* UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));*/
UARTStdioConfig(0, 57600, 16000000);
ROM_IntEnable(INT_UART0);
ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);
// IntPrioritySet(INT_UART0,0x00);
}
楼主请使用C:\ti\TivaWare_C_Series-2.1.0.12573\examples\boards\ek-tm4c123gxl\uart_echo这个例程的做法对UART进行初始化,接收使用中断方式,发送使用:
//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
//
ROM_UARTCharPutNonBlocking(UART0_BASE, *pui8Buffer++);
}
}
不要在中断中使用UARTprintf