官方有相关的例程吗,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
贴个内部Flash和EEPROM的读写例程:
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_types.h"
#include "inc/hw_memmap.h"
#include "driverlib/sysctl.h"
#include "driverlib/pin_map.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/flash.h"
#include "driverlib/eeprom.h"
int main(void)
{
uint32_t pui32Data[2];
uint32_t pui32Read[2];
pui32Data[0] = 0x12345678;
pui32Data[1] = 0x56789abc;
SysCtlClockSet(SYSCTL_SYSDIV_5|SYSCTL_USE_PLL|SYSCTL_XTAL_16MHZ|SYSCTL_OSC_MAIN);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x00);
SysCtlDelay(20000000);
FlashErase(0x10000);
FlashProgram(pui32Data, 0x10000, sizeof(pui32Data));
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x02);
SysCtlDelay(20000000);
SysCtlPeripheralEnable(SYSCTL_PERIPH_EEPROM0);
EEPROMInit();
EEPROMMassErase();
EEPROMRead(pui32Read, 0x0, sizeof(pui32Read));
EEPROMProgram(pui32Data, 0x0, sizeof(pui32Data));
EEPROMRead(pui32Read, 0x0, sizeof(pui32Read));
GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 0x04);
while(1)
{
}
}