This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123的GPIO中断问题

#include <stdbool.h>
#include <stdint.h>

#include "Key_Board.h"
#include "Nokia5110.h"
#include "SystemInit.h"

#include "driverlib/gpio.h"
#include "driverlib/sysctl.h"
#include "driverlib/interrupt.h"
#include "driverlib/timer.h"

#include "inc/hw_timer.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_gpio.h"
#include "inc/hw_sysctl.h"

unsigned char num;    //用来显示字符计数
unsigned char Int_flag=1; //中断标志位
unsigned char num2=0;   //负责对输入的计数
unsigned char key_val=88; //输入的值初始设置
unsigned char in_put_end_flag=0;//输入结束标志
unsigned char keyinput_val[]="A321B654C987DE0F";
unsigned char input[32];//输入的要显示的数组

/*********************************************************************************************************
** Function name:       GPIO_Port_F_ISR
** Descriptions:        GPIOF的中断服务函数
** input parameters:    无
** output parameters:   无
** Returned value:      无
*********************************************************************************************************/
void GPIO_Port_F_ISR(void)
{
 unsigned long ulStatus;
 unsigned char K_In;
 
 K_In=0x80; 
 SysCtlDelay(5*(TheSysClock/ 3000));   //消抖
 ulStatus=GPIOIntStatus(KEY_PORTF,true); // 读取中断状态
 GPIOIntClear(KEY_PORTF, ulStatus); // 清除中断状态,重要
 if (ulStatus&KEY_PIN_L)     //如果KEY_L的中断状态有效
 {
  SysCtlDelay(5*(TheSysClock/ 3000)); // 延时约10ms,消除松键抖动
  key_val=KeyIn(K_In); //读取按键值 
  KeyChecKend();//检查按键结束
 }
 Int_flag=0; 
 Nokia5110_DisNumber(0,5,key_val);
}

void Key_IntInit(void)
{
 /*高4位KEY_PIN_H配置*/
 {
  /*KEY_PIN_H使能*/
  SysCtlPeripheralEnable(KEY_PERIPH_GPIOC);  //高4位使能
  
  /*高4位KEY_PIN_H模式*/
  GPIOPinTypeGPIOOutput(KEY_PORTC,KEY_PIN_H);//高4为输出
  GPIOPinWrite(KEY_PORTC,KEY_PIN_H,0x00);  //高4位输出0
 }
 /*低4位中断输入设置*/
 {
  /*使能KEY_PIN_L所在GPIO端口*/
  SysCtlPeripheralEnable(KEY_PERIPH_GPIOF); //低4位使能
  HWREG(GPIO_PORTF_BASE + GPIO_O_LOCK) = 0x4c4f434b; //解锁PF0      
    HWREG(GPIO_PORTF_BASE + GPIO_O_CR) = GPIO_PIN_0;       

  /*设置KEY_PIN_L所在GPIO端口输入模式*/
  //GPIOPinTypeGPIOInput(KEY_PORTF,KEY_PIN_L);//低4位输入
  GPIOPadConfigSet(GPIO_PORTF_BASE,KEY_PIN_L,GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
    GPIODirModeSet(GPIO_PORTF_BASE,KEY_PIN_L, GPIO_DIR_MODE_IN);
  
  /*设置KEY_PIN_L中断类型*/
  GPIOIntTypeSet(KEY_PORTF,KEY_PIN_L,GPIO_FALLING_EDGE);//低4位下降沿触发中断
  //IntPrioritySet(INT_GPIOF, 1 << 5); // 设置KEY中断优先级为1
  
  /*注册中断*/
  GPIOIntRegister(KEY_PORTF,GPIO_Port_F_ISR);
 
  /*中断配置*/
  GPIOIntEnable(KEY_PORTF,KEY_PIN_L);//低4位中断输入使能 
  IntEnable(INT_GPIOF);
 }
}
/*********************************************************************************************************
** Function name:       Keycheckend
** Descriptions:        检查按键结束
** input parameters:    无
** output parameters:   无
** Returned value:      无
*********************************************************************************************************/
void KeyChecKend(void)
{
 SysCtlDelay(10 * (TheSysClock/ 3000)); // 延时约10ms,消除按键抖动
 //while (GPIOPinRead(KEY_PORTF,KEY_PIN_L) == 0x00); // 等待KEY抬起
 SysCtlDelay(10*(TheSysClock/ 3000)); // 延时约10ms,消除松键抖动
}
/*********************************************************************************************************
** Function name:       KeyIn
** Descriptions:       按键值检测模块
** input parameters:    无
** output parameters:   检测到的键盘输入值 key_val
** Returned value:      无
*********************************************************************************************************/
unsigned char KeyIn(unsigned char K_In) 
{
  unsigned char keyH_out;
  unsigned char temp1;
  unsigned char row;
  unsigned char col;
  unsigned char pinStatus;
 
  for(row=0;row<4;row++)
  {
   keyH_out=0xF0;
   keyH_out-=K_In;
   K_In>>=1;
   GPIOPinWrite(KEY_PORTC, KEY_PIN_H,keyH_out);
   pinStatus=GPIOPinRead(KEY_PORTF,KEY_PIN_L);
   if((pinStatus&0x0f)<0x0f)
   {
    temp1=0x01;
    for(col=0;col<4;col++)
    {
     if((pinStatus&temp1)==0x00)
     {
      key_val=col+row*4;      
     }
     temp1<<=1;
    }
   }    
  }
  GPIOPinWrite(KEY_PORTC, KEY_PIN_H,0x00);
  return  key_val;  
}

//主函数(程序入口)

int main(void)
{
 SysCtlClockSet(SYSCTL_SYSDIV_4 |
         SYSCTL_USE_PLL  |
         SYSCTL_OSC_MAIN |
         SYSCTL_XTAL_16MHZ);//配置为PLL 4分频,外部16Mhz晶振,则系统时钟为200Mhz/4=50Mhz
 Nokia5110_Init();    //液晶初始化
 Key_IntInit(); // KEY中断初始化
 //GPIOIntClear(KEY_PORTF, KEY_PIN_L); // 清除中断状态,重要
 IntMasterEnable(); // 使能处理器中断
 
 while(1)
 {
  
  Nokia5110_DisNumber(0,0,key_val);
  Nokia5110_DisNumber(0,1,1);
 }

// while(1) // 等待按键中断
// {
//  Nokia5110_DisNumber(0,5,key_val+1);
//  if(Int_flag==0)
//  {
//   Nokia5110_DisNumber(0,3,Int_flag);
//   Nokia5110_DisNumber(0,2,Int_flag);
//    if(key_val<15&&(key_val>0|| key_val==0))
//   {
//    Nokia5110_DisNumber(0,0,key_val);
//    input[num2]=keyinput_val[key_val];
//   }
//   Int_flag=1;
//   num2++;
//   if(key_val==0x0F)
//   {
//    num2=0;
//      Nokia5110_Dis6x8(0,0,input);
//   }
//   }
// }
} 

 上面的程序进入中断后,就在中断里面循环,出不来。不知到时怎么回事? 我看了一下硬件图发现WAKE引脚和按键硬件PF0连在一起,猜想是不是有影响