This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

M4内部ADC多路数据采集,数据顺序混乱



使用M4的内部ADC采集两路数据,一个接地,一个接3V,使用序列0,采集到的数据放到一个8元素数组中。。采集到的值大小正常,但就是在数组中放置的顺序是随机的,完全没有规律。。不知道是哪里出了问题,希望了解的人帮忙解答下。。
下面是ADC的配置函数

void ADCInit(void)
{

        //多通道。。。。。
        SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);

        SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
        GPIOPinTypeADC(GPIO_PORTE_BASE,GPIO_PIN_3|GPIO_PIN_2);

        ADCReferenceSet(ADC0_BASE,ADC_REF_INT);
        ADCSequenceConfigure(ADC0_BASE,SEQ_NUM,ADC_TRIGGER_TIMER,0);//每10us触发一次
//        ADCSequenceConfigure(ADC0_BASE,SEQ_NUM,ADC_TRIGGER_ALWAYS,0);
//        ADCSequenceConfigure(ADC0_BASE,SEQ_NUM,ADC_TRIGGER_PROCESSOR,0);
        ADCSoftwareOversampleConfigure(ADC0_BASE,SEQ_NUM,64);
        ADCSequenceStepConfigure(ADC0_BASE,SEQ_NUM,0,ADC_CTL_CH1);
        ADCSequenceStepConfigure(ADC0_BASE,SEQ_NUM,1,ADC_CTL_CH1);
        ADCSequenceStepConfigure(ADC0_BASE,SEQ_NUM,2,ADC_CTL_CH1);
        ADCSequenceStepConfigure(ADC0_BASE,SEQ_NUM,3,ADC_CTL_CH1);
        ADCSequenceStepConfigure(ADC0_BASE,SEQ_NUM,4,ADC_CTL_CH0);
        ADCSequenceStepConfigure(ADC0_BASE,SEQ_NUM,5,ADC_CTL_CH0);
        ADCSequenceStepConfigure(ADC0_BASE,SEQ_NUM,6,ADC_CTL_CH0);
        ADCSequenceStepConfigure(ADC0_BASE,SEQ_NUM,7,ADC_CTL_CH0| ADC_CTL_IE | ADC_CTL_END);


        ADCSequenceEnable(ADC0_BASE, SEQ_NUM);

        ADCIntRegister(ADC0_BASE,SEQ_NUM,ADC0IntHander);
        ADCIntClear(ADC0_BASE,SEQ_NUM);
        ADCIntEnable(ADC0_BASE,SEQ_NUM);
}

下面是中断函数:

void ADC0IntHander(void)
{
        uint32_t temp[8] = {0};
        ADCSequenceDataGet(ADC0_BASE,SEQ_NUM,temp);
        ADCIntClear(ADC0_BASE,SEQ_NUM);//设置断点。。
}