This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C129ENCPDT的SPI发送数据时,TX端口和CLK端口都没有波形

Other Parts Discussed in Thread: TM4C129ENCPDT

如题,我现在在用TM4C129ENCPDT的SSI模块做SPI通信,在发送数据的时候TX和CLK端口都没有波形。芯片外的所有器件已经全部拆掉,程序初始化如下:


SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI2);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);


GPIOPinConfigure(GPIO_PD0_SSI2XDAT1);
GPIOPinConfigure(GPIO_PD1_SSI2XDAT0);
GPIOPinConfigure(GPIO_PD2_SSI2FSS);
GPIOPinConfigure(GPIO_PD3_SSI2CLK);
GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);


SSIDisable(SSI2_BASE);


SSIConfigSetExpClk(SSI2_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0,
SSI_MODE_MASTER, 1200000, 8);


SSIIntClear(SSI2_BASE, 0xffff); 
IntEnable(INT_SSI2); 

SSIIntEnable(SSI2_BASE, SSI_RXTO | SSI_RXOR); //SSIÖжÏÑÚÂëʹÄÜ
SSIIntDisable(SSI2_BASE,SSI_TXFF | SSI_RXFF);


SSIEnable(SSI2_BASE);