Part Number: MSP432-DEBUGGERS
Hello everyone, I am using the MSP432P401Rlaunchpad development board here, after I opened it, my idea is to use kielMDK for development, and the environment has been built, after I power up the development board, I use the Windows environment, all DAPdebugger can be used, and the address can be read by using debug in MDK, but the emulator does not work normally after I switch to TI XDS, I would like to ask what I should do to reuse DAPdebugger?
大家好,我这里使用的是MSP432P401Rlaunchpad开发板,我开封了之后我的想法是使用kielMDK进行开发,同时环境已经搭建完成了,我给开发板上电了之后,使用的是Windows环境,所有DAPdebugger可以使用,在MDK里面使用debug也能读取到地址,但是我切换到TI XDS之后仿真器不能正常工作了,重启之后也是保持这个状态,我想请问一下应该怎么做我才能重新使用DAPdebugger呢?