This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在使用MSP432P401R的时候,遇到一些关于MCLK和SMCLK的问题,当我将两个时钟设置为不同的频率时,使用Timer0产生PWM时,会偶尔会出现PWM没有输出的情况
MCLK=48MHz,SMCLK=24MHz
我想问题一下,MSP432P401R资料里面,是否包含MSP430系列勘误表中PMM32的同样内容,因为相关文档和资料已经在官网上查不到内容了
MSP432P401R的Errata中不包含同样的内容。
我也具体看了一下Errata PMM32,和你遇到的问题关联似乎并不大。
首先PMM32是从active mode切换到 低功耗模式2/3/4 的时候可能会出现;其次Timer在配置完成以后,是自己在运行的,与CPU无关。
另外MCLK也输入不到Timer中。