,用的芯片型号是TM4C129XNCZAD。ADCSequenceStepConfigure(ADC0_BASE, 0, 0, ADC_CTL_CH0 | ADC_CTL_IE);为什么只能输出ADC_CTL_CH0到ADC_CTL_CH7,ADC_CTL_CH8到ADC_CTL_CH23无数值输出,查看资料,发现以前的LM3S9B96芯片只能初始化到ADC_CTL_CH7,是不是由于ADCSequenceStepConfigure()函数未更新造成的,如果是,怎么在底层修改ADCSequenceStepConfigure()函数。
ADCSequenceStepConfigure()函数如下所示:
#define ADC_SEQ (ADC_O_SSMUX0)
#define ADC_SEQ_STEP (ADC_O_SSMUX1 - ADC_O_SSMUX0)
#define ADC_SSMUX (ADC_O_SSMUX0 - ADC_O_SSMUX0)
#define ADC_SSEMUX (ADC_O_SSEMUX0 - ADC_O_SSMUX0)
#define ADC_SSCTL (ADC_O_SSCTL0 - ADC_O_SSMUX0)
#define ADC_SSFIFO (ADC_O_SSFIFO0 - ADC_O_SSMUX0)
#define ADC_SSFSTAT (ADC_O_SSFSTAT0 - ADC_O_SSMUX0)
#define ADC_SSOP (ADC_O_SSOP0 - ADC_O_SSMUX0)
#define ADC_SSDC (ADC_O_SSDC0 - ADC_O_SSMUX0)
void
ADCSequenceStepConfigure(uint32_t ui32Base,uint32_t ui32SequenceNum
uint32_t ui32Step,uint32_t ui32Config)
{
uint32_t ui32Temp;
ASSERT((uint32_t ui32Base == ADC0_BASE)||(uint32_t ui32Base == ADC1_BASE));
ASSERT(ui32SequenceNum<4);
ASSERT(((ui32SequenceNum == 0) && (ui32Step < 8))||
((ui32SequenceNum == 1) && (ui32Step < 4))||
((ui32SequenceNum == 2) && (ui32Step < 4))||
((ui32SequenceNum == 3) && (ui32Step < 1)));
ui32Base +=ADC_SEQ + (ADC_SEQ_STEP * ui32SequenceNum);
ui32Step *= 4;
HWREG(ui32Base + ADC_SSMUX) = ((HWREG(ui32Base + ADC_SSMUX) &
~(0x0000000f << ui32Step)) |
((ui32Config & 0x0f) << ui32Step);
HWREG(ui32Base + ADC_SSEMUX) = (HWREG(ui32Base + ADC_SSeMUX) &
~(0x0000000f << ui32Step)) |
(((ui32Config & 0xf00) >>8) << ui32Step);
HWREG(ui32Base + ADC_SSCTL) = ((HWREG(ui32Base + ADC_SSCTL) &
~(0x0000000f << ui32Step)) |
(((ui32Config & 0xf0) >>4) << ui32Step);
if(ui32Config & 0x000F0000)
{
ui32Temp = HWREG(ui32Base + ADC_SSDC);
ui32Temp &= ~(0xF << ui32Step);
ui32Temp |= (((ui32Config & 0x00070000) >> 16) << ui32Step);
HWREG(ui32Base + ADC_SSDC) = ui32Temp;
HWREG(ui32Base + ADC_SSOP) |= (1 << ui32Step);
}
else
HWREG(ui32Base + ADC_SSOP) &= ~(1 << ui32Step);
}