This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS470MF03107: PWM signals' period(& duty) generation based on HET displayed on Oscilloscope screen is very different from period(& duty) set in CCS project files generated from HALCogen.

Part Number: TMS470MF03107


tms470mf03107 HET module pin description:

 

PCB 4 PWM pin layout:

 

After ZOOM in:

 

HET Global Timing Configuration is as follows:

The main function is as follows:

int main(void)

{

/* USER CODE BEGIN (2) */

    hetInit();

            pwmSetSignal(pwm0,set_pwm0);

            pwmSetSignal(pwm1,set_pwm1);

            pwmSetSignal(pwm2,set_pwm2);

            pwmSetSignal(pwm3,set_pwm3);

           // pwmSetSignal(pwm4,set_pwm4);

           // pwmSetSignal(pwm5,set_pwm5);

           // pwmSetSignal(pwm6,set_pwm6);

           // pwmSetSignal(pwm7,set_pwm7);

 

            pwmStart(pwm0);

            pwmStart(pwm1);

            pwmStart(pwm2);

            pwmStart(pwm3);

           // pwmStart(pwm4);

           // pwmStart(pwm5);

           // pwmStart(pwm6);

          //  pwmStart(pwm7);

 

            pulse_pwm0 = pwmGetSignal(pwm0);

            pulse_pwm1 = pwmGetSignal(pwm1);

            pulse_pwm2 = pwmGetSignal(pwm2);

            pulse_pwm3 = pwmGetSignal(pwm3);

          //  pulse_pwm4 = pwmGetSignal(pwm4);

          //  pulse_pwm5 = pwmGetSignal(pwm5);

           // pulse_pwm6 = pwmGetSignal(pwm6);

           // pulse_pwm7 = pwmGetSignal(pwm7);

//        }

/* USER CODE END */ 

}

4 PWM signal Period set is the same with the PWM signals generated by program,covering the minimum(482us) and maximum period(1736044us) i want.

BUT the real PWM signal waves are as follows:

S1(PWM0,het[11]):

Constantly HIGH level:

S2(PWM1,het[12]):

displayed PWM wave output period is 290us,which is HALF of the set period 578us:

 

 

S3(PWM2,het[13]):

displayed PWM wave output period is 720ms,which is HALF of the set period 1446703us:

 

 

S4(PWM3,het[14]):

displayed PWM wave output period is 880ms,which is HALF of the set period 1736044us

 

 

When the global timing configuration is as follows,which is default setting(other configuration stays the same):

 

PWM0 and PWM1 period set is the same with the program-generated value,but program-generated value of PWM2 and PWM3 duty&period are abnormal compared with the duty&period set.You can see as follows:

 

Oscilloscope Screen displays are as follows:

S1:period=960us,TWICE of the set period 480us

 

S2:period=1160us,TWICE if the set period 578us

 

S3:almost constant level 376ms TWICE of 188414us

 

S4:duty abnormal, constant HIGH level:

Here in order for simplification, some other test and description is as follows:

HET Global Timing Configuration ONE:

 

4 PWM signal Period set is 10000us(10ms),which is the same with the PWM signals generated:  

 

But the real PWM pulse waves are as follows:

S1(PWM0,het[11]):NO PWM wave shape displayed on Oscilloscope screen,but pulled HIGH constantly.

 

S2(PWM1,het[12]),S3(PWM2,het[13]),S4(PWM3,het[14]):PWM waves are displayed as follows on screen,but pulse period(5000us or 5ms) is HALF of the set period(10000us or 10ms):

 

 

WHEN the global timing configuration TWO is as follows:

 

4 PWM signal Period set is 10000us(10ms),which is the same with the PWM signals generated:

 

 

But the real 4 PWM pulse waves are as follows,all having high and low level apparently,but pulse period(20000us or 20ms) is TWICE of the set period(10000us or 10ms).

 

All in all, I wonder, based on the certain HET timing configuration, why the generated  PWM periods are not the same with the PWM period(& duty) set by me. Please make an answer as in detail as possible.

THX~!