This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

系统休眠问题死机(Powerdomain (neon_pwrdm) didn't enter target state 0)



557] Freezing user space processes ... (elapsed 0.02 seconds) done. [   35.113494] Freezing remaining freezable tasks ... (elapsed 0.02 seconds) done. [   35.146423] Suspending console(s) (use no_console_suspend to debug) [   35.161437] PM: suspend of devices complete after 8.087 msecs [   35.161773] PM: late suspend of devices complete after 0.305 msecs [   35.328704] Powerdomain (neon_pwrdm) didn't enter target state 0 [   35.328735] Could not enter target state in pm_suspend [   35.329010] PM: early resume of devices complete after 0.183 msecs [   35.329345] platform iva.0: omap_voltage_scale: Already at the requestedrate 800000000 [   35.329345] platform mpu.0: omap_voltage_scale: Already at the requestedrate 1000000000 [   35.332855] powerbutton_irq err=0 value=0x51   value_cfg_p1=0xff    value_p1_sw=0x18  [   35.332916] wakeup wake lock: event2-1154 [   35.380279] PM: resume of devices complete after 51.177 msecs [   35.447082] Restarting tasks ... done. [   35.462982] suspend: exit suspend, ret = 0 (2000-01-01 00:00:31.582855225 UTC) [   35.478302] request_suspend_state: wakeup (3->0) at 35693021288 (2000-01-01 00:00:31.598175049 UTC)

  • 这......

    能详细说明下您的问题吗

  • Powerdomain(neon_pwrdm)没有输入目标状态0

    557]冻结用户空间进程……(经过0.02秒)。[35.113494]冻结剩余冻任务……(经过0.02秒)。[35.146423]暂停控制台(s)(用no_console_suspend调试)(35.161437)下午:暂停设备的完整后8.087毫秒断开(35.161773)下午:暂停后期的设备完成后0.305毫秒断开[35.328704]Powerdomain(neon_pwrdm)没有进入目标状态0[35.328735]不能在pm_suspend输入目标状态(35.329010)下午:早期恢复的设备完成后0.183毫秒断开iva[35.329345]平台。0:omap_voltage_scale:已经在requestedrate 800000000[35.329345]平台微处理器。0:omap_voltage_scale:已经在requestedrate 1000000000[35.332855]powerbutton_irq呃= 0值= 0 x51 value_cfg_p1 = 0 xff value_p1_sw = 0 x18[35.332916]唤醒后锁:event2 - 1154(35.380279)下午:简历的设备完成后51.177毫秒断开[35.447082]重启任务……完成了。[35.462982]暂停:出口暂停,ret = 0(2000-01-01 00:00:31.582855225 UTC)[35.478302]request_suspend_state:唤醒(3 - > 0)35693021288(2000-01-01 00:00:31.598175049 UTC)

    楼主你这个问题很严重啊,你不说清楚我们不好抓药