This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.当前R5主频为400MHZ,在手册描述中写到EPWM是属于CONTROLSS模块,那么我是否应该去配置CONTROLSS_PLL_CLK_SRC_SEL选择为DPLL_CORE_HSDIV0_CLKOUT2(400MHZ),然后PWM的分频系数为1,那么我的PWM的基频就是400MHZ吗?
2.导入demo工程epwm_hr_duty_cycle_am263x-cc_r5fss0-0_nortos_ti-arm-clang,出来的PWM周期为1ms,1Khz,然后分频系数DIV是4,updowm模式计数是25000,那么我反推算PWM的输入时钟应为200MHZ,debug时CONTROLSS时钟配置如图,从寄存器配置看CONTROLSS时钟为400MHZ,为何反推算时200MHZ?我看到SYS_CLK为200MHZ,PWM输入时钟是SYS_CLK吗?
然后PWM的分频系数为1,那么我的PWM的基频就是400MHZ吗?
对的
从寄存器配置看CONTROLSS时钟为400MHZ,为何反推算时200MHZ?我看到SYS_CLK为200MHZ,PWM输入时钟是SYS_CLK吗?
是因为PWM模块的时钟来源不一定是CONTROLSS模块的时钟,而是可能被设置为SYS_CLK,或者在配置时经过了其他的分频。PWM输入时钟可能是SYS_CLK的某个分频
PWM 模块的源时钟是 SYS_CLK (200 MHz)。CONTROLSS_PLL_CLK (400 MHz) 专门用于 CONTROLSS 内的 FSI 和 SDFM 模块。
您希望保留 200 MHz SYS_CLK(这对于整体器件时序/时钟至关重要)并修改 PWM 模块内的计数器/选项以降低频率以满足应用要求?