This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

清华大学TM4C123微处理器原理与实践例程-UART实验程序解析



//UART实验程序解析
//头文件
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/debug.h"
#include "driverlib/fpu.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/rom.h"
#include "driverlib/pin_map.h"

//串口接收中断服务程序
void UARTIntHandler(void)
{
  ui32 ulStatus;
  //获取中断状态
  ulStatus = ROM_UARTIntStatus(UART0_BASE, true);
  //清除中断标志
  ROM_UARTIntClear(UART0_BASE, ulStatus);
  //直到串口FIFO中没有数据时才退出循环
  while(ROM_UARTCharsAvail(UART0_BASE))
  {
      //读串口接收的字符并回发
      ROM_UARTCharPutNonBlocking(UART0_BASE,
             ROM_UARTCharGetNonBlocking(UART0_BASE));
  }
 }

//串口发送函数
void  UARTSend(const ui8 *pucBuffer, ui32 ulCount)
{
  while(ulCount--)
  {
      //将要发送的字符写进UART
      ROM_UARTCharPutNonBlocking(UART0_BASE, *pucBuffer++);
  }
}

int main(void)
{
  //使能FPU
  FPUEnable();
  FPULazyStackingEnable();

  //设置时钟直接使用外部晶振
  ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | 
                SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);

  //使能用到的外设
  ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
  ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
  //配置PA0和PA1为串口0引脚
  ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | 
                         GPIO_PIN_1);

  //使能中断
  ROM_IntMasterEnable();

  //配置UART0为115200,8-N-1
  ROM_UARTConfigSetExpClk(UART0_BASE, ROM_SysCtlClockGet(), 
                            115200,	 (UART_CONFIG_WLEN_8 | 
          UART_CONFIG_STOP_ONE | UART_CONFIG_PAR_NONE));
  //使能串口中断
  ROM_IntEnable(INT_UART0);
  ROM_UARTIntEnable(UART0_BASE, UART_INT_RX | UART_INT_RT);
  //发送提示信息
  UARTSend((ui8 *)"Enter text: \r", 13);

  while(1)
  {
   }
  }