This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TF 卡访问问题

Other Parts Discussed in Thread: AM3352

使用TI的AM3352主芯片,软件从TF卡启动,在软件启动过程中运行实时LINUX系统,如果TF卡上COPY过一个任意文件,开机运行时会出现如下错误,该如何解决?

 [    0.329421] <pluse-drv>: bus_base_addr0 0xe3000000, bus_base_addr1 0xe5000000
.
[    0.337024] <pluse-drv>: rtdm_dev_register 0.
[    0.341667] <etc-drv>: rtdm_dev_register 0.
[    0.432542] Missing dual_emac_res_vlan in DT.
[    0.437172] Using 1 as Reserved VLAN for 0 slave
[    0.442047] Missing dual_emac_res_vlan in DT.
[    0.446615] Using 2 as Reserved VLAN for 1 slave
[    0.459985] ec_generic: Binding socket to interface 5 (eth1).
[    2.032992] systemd-fsck[81]: fsck failed with error code 4.
[    2.130878] systemd-udevd[86]: worker [97] did not accept message -1 (Connect
ion refused), kill it
[    2.161653] systemd-udevd[86]: worker [99] did not accept message -1 (Connect
ion refused), kill it
[    2.181404] systemd-udevd[86]: worker [101] did not accept message -1 (Connec
tion refused), kill it
Welcome to emergency mode! After logging in, type "journalctl -xb" to view
system logs, "systemctl reboot" to reboot, "systemctl default" to try again
to boot into default mode.

Give root password for system maintenance
(or type Control-D for normal startup):