芯片手册电源和时钟部分,operating performance points (OPPs) 是什么意思?谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
芯片手册电源和时钟部分,operating performance points (OPPs) 是什么意思?谢谢
工作点的意思吧,字面意思是,操作执行点,结合上下文,大概就是当使用这个ZCZ封装选项的时候,VDD MPU和VDD CORE电源输入可以是来自同一个电源,如果应用程序只是使用通用电源为VDD_MPU 和 VDD_CORE提供的电压作为工作点的话。
------------------------------------------------
When using the ZCZ package option, VDD_MPU and VDD_CORE power inputs may be powered from the same source if the application only uses operating performance points (OPPs) that define a common power supply voltage for VDD_MPU and VDD_CORE.
------------------------------------
楼主觉得我这解释的还行吧。