之前我问过用P1口驱动液晶不行,但是P2口就可以使用,现在我进一步发现使用P1.0,P1.1,P1.2,P1,5驱动不行,但是使用P1.0,P1.1,P1.3,P1.5就可以驱动,这就表明了是P1.2的问题,于是问题到底是什么?希望知道者能告知。谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前我问过用P1口驱动液晶不行,但是P2口就可以使用,现在我进一步发现使用P1.0,P1.1,P1.2,P1,5驱动不行,但是使用P1.0,P1.1,P1.3,P1.5就可以驱动,这就表明了是P1.2的问题,于是问题到底是什么?希望知道者能告知。谢谢!!!
没有端口复用都是只是配置了IO口应该不是驱动能力的问题吧,其他口都能用我用了4个口通信,只有用了P1.2口就不行,没用就可以通信。就这个问题好无奈
作为测试,你可以这样,你独立的对P1.2,进行IO测试,作为一个闪灯测试,delay延时0.5s,然后看能否驱动的起来。