目前打算用TM4C129做开发,因为其性能比123好,但是129手头的资料少。打算买一本《TM4C123微处理器原理与实践》作为129开发的参考,不知道是不是可行?
另外,原先做STM32开发时,ST有官方函数库可以选用,不知道TI有没有?是否是TIVAWARE?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前打算用TM4C129做开发,因为其性能比123好,但是129手头的资料少。打算买一本《TM4C123微处理器原理与实践》作为129开发的参考,不知道是不是可行?
另外,原先做STM32开发时,ST有官方函数库可以选用,不知道TI有没有?是否是TIVAWARE?
TM4C123的源代码,能不能直接在TM4C129之上直接运行?
这个没试过,应该是不可以的。两者的外设差不多,库函数的名称的差不多,你可以对照着写。
这个是不可以的,你可以下载TIVAWARE,再买一个相应的评估板,就可以动手了。关于123x和129x的区别,分享个文章给你 an01296 Differences Between TM4C123x and TM4C129x MCUs,见附件
你仔细对比下,会发现123x和129x在QEI上差别并不大。两者主频,外设相差较大,ov7670没有用过。
搭载ov7670/7620的摄像头,123足够了,M3都可以实现的,M4也可以,129系列主打的是以太网,如果用不到这个,选123就可以。129的主频也比123的高。
我之前用STM32F103系列的搭载摄像头,速度就很吃力,完全不能达到我的要求。
STM32的的最高主频为72MHZ,123系列的最高主频为80MHZ,也大不了多少的。129系列的最高主频为120MHZ,那么你可以试试这个。你可以先用STM32的超频试试。
STM32是M3的内核,TM4C123/129是M4F的内核,支持的指令集和处理能力都有提升