您好!我正在尝试实现TIDA-01527项目。根据实际要求,我需要生成10kHz的正弦激励信号。参考之前的社区问答内容以及设计文档,我了解到首先需要将TIDA-01527CCS工程中resolver.h文件内的EXC_STEPS_PER_PERIOD 64 /* 2^6 -> 6-bit resolution per EXC period */一行程序中的64修改为32。除此之外,是否还需要将下图所示的由PWM信号生成EXC_P与EXC_N滤波电路的截止频率进行修改?我尝试使用了您之前提到的在线计算工具网页http://sim.okawa-denshi.jp/en/OPtazyuLowkeisan.htm,使用了20kHz作为截止频率,同时保持了C3与C4的值与原设计相同,如下图所示请问该计算是否正确?此外还有哪些地方需要进行修改呢?期待您的尽早回复。