This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于MSP432的FPU的问题



我用这个程序测试FPU效果,现在程序时一次加上FPU_enableModule(),一次不加,可是发现两次P1.0的LED闪烁的频率完全一样,好像FPU没有作用,为什么??

/* DriverLib Includes */
#include "driverlib.h"

/* Standard Includes */
#include <stdint.h>
#include <stdbool.h>
#include <math.h>

int main(void)
{
	volatile float fCalculate;
	uint32_t ii;
	flipFlop = false;
    /* Stop Watchdog  */
    MAP_WDT_A_holdTimer();
    MAP_GPIO_setAsOutputPin(GPIO_PORT_P1,GPIO_PIN0);
//  FPU_enableModule();
    while(1)
    {
        GPIO_toggleOutputOnPin(GPIO_PORT_P1,GPIO_PIN0);
        for(ii=0;ii<20;ii++)
               {
        	fCalculate = (sin(50.5) * (12.2f / 50.1f) * 10.22f / 3) * ii;
               }
    }
}
  • /*
     * -------------------------------------------
     *    MSP432 DriverLib - v01_04_00_18 
     * -------------------------------------------
     *
     * --COPYRIGHT--,BSD,BSD
     * Copyright (c) 2015, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     * --/COPYRIGHT--*/
    /*******************************************************************************
     * MSP432 FPU - Simple FPU Operation
     *
     * Description: In this barebone example, the FPU is enabled and the
     * effectiveness of the FPU with respect to floating point math is examined
     * versus having the FPU disabled. A perpetual while loop is set up that
     * continuously does floating point calculation. When the push button
     * attached to P6.7 is pressed, the FPU is enabled/disabled. This shows
     * the user the power consumption differences when having the FPU enabled
     * versus having the FPU disabled. Less cycle counts mean the user can enter a
     * low power mode quicker.
     *
     *                MSP432P401
     *             ------------------
     *         /|\|                  |
     *          | |                  |
     *          --|RST               |
     *            |                  |
     *            |            P1.1  |<--Toggle Switch
     *            |                  |
     *            |                  |
     *
     * Author: Timothy Logan
     ******************************************************************************/
    /* DriverLib Includes */
    #include "driverlib.h"
    
    /* Standard Includes */
    #include <stdint.h>
    
    #include <stdbool.h>
    #include <math.h>
    
    /* Statics */
    static volatile bool flipFlop;
    
    int main(void)
    {
        volatile float fCalculate;
        uint32_t ii;
        flipFlop = false;
    
        MAP_WDT_A_holdTimer();
    
        /* Configuring P1.1 as an input and enabling interrupts */
        MAP_GPIO_setAsInputPinWithPullUpResistor(GPIO_PORT_P1, GPIO_PIN1);
        MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, GPIO_PIN1);
        MAP_GPIO_enableInterrupt(GPIO_PORT_P1, GPIO_PIN1);
        MAP_Interrupt_enableInterrupt(INT_PORT1);
        MAP_Interrupt_enableMaster();
    
        while(1)
        {
            for(ii=0;ii<20;ii++)
            {
                fCalculate = (sin(50.5) * (12.2f / 50.1f) * 10.22f / 3) * ii;
            }
        }
    }
    
    /* GPIO ISR */
    void gpio_isr(void)
    {
        uint32_t status;
    
        status = MAP_GPIO_getEnabledInterruptStatus(GPIO_PORT_P1);
        MAP_GPIO_clearInterruptFlag(GPIO_PORT_P1, status);
    
        /* Toggling the output on the LED */
        if(status & GPIO_PIN1)
        {
            if(flipFlop)
            {
                MAP_FPU_disableModule();
                flipFlop = false;
            }
            else
            {
                MAP_FPU_enableModule();
                flipFlop = true;
            }
        }
    
    }
    
  • 你另外一个添加关闭该模块功能试试看。

  • TI的这个例程是有问题的,在编译器的设置中开启FPU的情况下,调用FPU_disbleModule()函数会产生一个错误,并且这个例程看不出开启FPU的效果。

    具体请参考 https://e2e.ti.com/support/microcontrollers/msp430/f/166/p/413420/1470908