This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM46L852: RM46L852C RMII设计使用hdkif_transmit无法输出

Part Number: RM46L852


参考git://git.ti.com/hercules_examples/hercules_examples.git代码,验证RMII。实际使用hdkif_transmit接口无内容输出,TX_EN、TXD_0、TXD_0均没有信号输出。

  • 源码:

    static void
    hdkif_transmit(struct hdkif *hdkif, struct pbuf *pbuf) {
      struct pbuf *q;
      struct txch *txch;
      volatile struct emac_tx_bdp *curr_bd, *active_head, *bd_end;

      txch = &(hdkif->txch);
      /* Get the buffer descriptor which is free to transmit */
      curr_bd = txch->free_head;
     
      active_head = curr_bd;
     
      /* Update the total packet length */
      uint32 flags_pktlen = pbuf->tot_len;
      flags_pktlen |= (EMAC_BUF_DESC_SOP | EMAC_BUF_DESC_OWNER);
      curr_bd->flags_pktlen = hdkif_swizzle_data(flags_pktlen);

      /* Copy pbuf information into TX buffer descriptors */
      for(q = pbuf; q != NULL; q = q->next) {

        /* Intialize the buffer pointer and length */
        curr_bd->bufptr = hdkif_swizzle_data((uint32)(q->payload));
        curr_bd->bufoff_len = hdkif_swizzle_data((q->len) & 0xFFFF);
        bd_end = curr_bd;
        curr_bd->pbuf = pbuf;
        curr_bd = hdkif_swizzle_txp(curr_bd->next);
        //if (curr_bd) curr_bd->flags_pktlen = 0;
      }

      /* Indicate the end of the packet */
      bd_end->next = NULL;
      bd_end->flags_pktlen |= hdkif_swizzle_data(EMAC_BUF_DESC_EOP);
     
      txch->free_head = curr_bd;
     
      /* For the first time, write the HDP with the filled bd */
      if(txch->active_tail == NULL) {
        EMACTxHdrDescPtrWrite(hdkif->emac_base, (unsigned int)(active_head), 0);
      }
     
      /*
       * Chain the bd's. If the DMA engine, already reached the end of the chain,
       * the EOQ will be set. In that case, the HDP shall be written again.
       */
      else {
        curr_bd = txch->active_tail;
        /* TODO: (This is a workaround) Wait for the EOQ bit is set */
        while (EMAC_BUF_DESC_EOQ != (hdkif_swizzle_data(curr_bd->flags_pktlen) & EMAC_BUF_DESC_EOQ));
        /* TODO: (This is a workaround) Don't write to TXHDP0 until it turns to zero */
          while (0 != *((uint32 *)0xFCF78600));
        curr_bd->next = hdkif_swizzle_txp(active_head);
        if (EMAC_BUF_DESC_EOQ == (hdkif_swizzle_data(curr_bd->flags_pktlen) & EMAC_BUF_DESC_EOQ)) {
          /* Write the Header Descriptor Pointer and start DMA */
          EMACTxHdrDescPtrWrite(hdkif->emac_base, (unsigned int)(active_head), 0);
        }
      }

      txch->active_tail = bd_end;
    }

  • 您好,

          感谢您对TI产品的关注!
          为更加有效地解决您的问题,我们建议您将问题发布在E2E英文技术论坛上(e2e.ti.com),将由资深的英文论坛工程师为您提供帮助。