Other Parts Discussed in Thread: AFE4300
有没有谁对AFE4300测量人体电阻很熟悉的呀?我对他的测量原理不是很懂?还有就是应该怎样检测测量结果的准确性!官方给的3种模式的阻抗网络是什么意思呀?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: AFE4300
有没有谁对AFE4300测量人体电阻很熟悉的呀?我对他的测量原理不是很懂?还有就是应该怎样检测测量结果的准确性!官方给的3种模式的阻抗网络是什么意思呀?
AFE4300是怎样测量人体成分的呢?宋经理进行了详细阐述:“ AFE4300可以测量手到手、脚到脚甚至从手到脚之间,也就是人体四肢任何两个分支之间的阻抗。首先,它产生一个正弦波形去激励人体,把正弦波形加在两个测量点上,由于正弦波是一个交流信号,随着人体成分(人体脂肪)的不同,它的阻抗是不同的。而另外一个通道会采样和分析人体阻抗(它并不是一个纯的电阻形式,它还含有电感和电容,实际上是一个复合的阻抗),通过芯片内部的IQ分离和滤波,再通过一定的数字运算,得到了I和Q信号,这样就得到了两个测量点间的阻抗大小,可以在一定程度上反映人体成分。大家可以看到,对体成分前端的测量相对而言比较复杂,它包括四极测量技术和复数阻抗测量技术。当然,我们这个AFE4300只是把人体的阻抗数字化,并进行IQ分离,后续的工作交给MCU或者DSP进行处理。例如显示、到底多少阻抗配备多少的脂肪含量等。”
AFE4300内部结构图如图2所示。AFE4300 集成了两个单独的信号链,一个针对重量测量,另一个针对身体成分分析,二者之间采用16 bit 860 S/s 模数转换器(ADC) 进行多路复用。AFE4300的主要优势有:(1)高精度。AFE4300 的四极(tetra-polar) 测量技术可消除电极阻抗对准确度的影响。该器件的3 个BCM 通道可在手到手、脚到脚甚至从手到脚的整个身体间实现分段阻抗分析(BIA),提高整体测量精度。该器件还提供使用生物阻抗光谱(BIS) 准确测量细胞外液(ECW) 和细胞内液(ICW) 的选项。(2)极低功耗.AFE4300 流耗低于1 mA,电源电压范围在2 V ~ 3.6 V 之间,可延长电池使用寿命。(3)小体积。采用12 mm×12 mm TQFP-80 封装。此外,由于它是一个完整的前端解决方案,可以加快产品上市时间。

以市场为导向的AFE4300,虽然功能多、内部结构复杂,但是既然工程师们可以使用它来更加方便地设计产品,为什么不赶快行动呢?